[yocto]sgtl5000 hangs i2c bus after reset

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

[yocto]sgtl5000 hangs i2c bus after reset

1,091 次查看
charleshuang
Senior Contributor II

Hi

We use i.MX6D and sgtl5000 on fsl-yocto-3.10.17_1.0.0

We found a issue ,after play music and reboot device

I2C bus is hanged because of sgtl5000

I see other people have encountered the same problem

Re: SGTL5000 hangs I2C bus after reset

But the patch of answer ,can't apply our kernel version

Please help  to solve this issue

Thanks

0 项奖励
回复
3 回复数

637 次查看
igorpadykov
NXP Employee
NXP Employee

Hi charles

this link also mentions the same kernel patch for wandboard imx_3.10.17_1.0.0_ga

ASoC: sgtl5000: Fix the cache handling · wandboard-org/linux@55d6dfb · GitHub

Best regards

igor

0 项奖励
回复

637 次查看
charleshuang
Senior Contributor II

Hi

I try your patch,but I got kernel panic after playing music and reset my device

Attached is kernel message

thanks

0 项奖励
回复

637 次查看
igorpadykov
NXP Employee
NXP Employee

you are using customized advantech linux, so it may be

recommended to apply to them for modifications.

Alternatively one can debug it using AN4553

Using Open Source Debugging Tools for Linux on i.MX Processors

~igor

0 项奖励
回复