[yocto]sgtl5000 hangs i2c bus after reset

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[yocto]sgtl5000 hangs i2c bus after reset

1,090 Views
charleshuang
Senior Contributor II

Hi

We use i.MX6D and sgtl5000 on fsl-yocto-3.10.17_1.0.0

We found a issue ,after play music and reboot device

I2C bus is hanged because of sgtl5000

I see other people have encountered the same problem

Re: SGTL5000 hangs I2C bus after reset

But the patch of answer ,can't apply our kernel version

Please help  to solve this issue

Thanks

0 Kudos
Reply
3 Replies

636 Views
igorpadykov
NXP Employee
NXP Employee

Hi charles

this link also mentions the same kernel patch for wandboard imx_3.10.17_1.0.0_ga

ASoC: sgtl5000: Fix the cache handling · wandboard-org/linux@55d6dfb · GitHub

Best regards

igor

0 Kudos
Reply

636 Views
charleshuang
Senior Contributor II

Hi

I try your patch,but I got kernel panic after playing music and reset my device

Attached is kernel message

thanks

0 Kudos
Reply

636 Views
igorpadykov
NXP Employee
NXP Employee

you are using customized advantech linux, so it may be

recommended to apply to them for modifications.

Alternatively one can debug it using AN4553

Using Open Source Debugging Tools for Linux on i.MX Processors

~igor

0 Kudos
Reply