[yocto]sgtl5000 hangs i2c bus after reset

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[yocto]sgtl5000 hangs i2c bus after reset

1,042件の閲覧回数
charleshuang
Senior Contributor II

Hi

We use i.MX6D and sgtl5000 on fsl-yocto-3.10.17_1.0.0

We found a issue ,after play music and reboot device

I2C bus is hanged because of sgtl5000

I see other people have encountered the same problem

Re: SGTL5000 hangs I2C bus after reset

But the patch of answer ,can't apply our kernel version

Please help  to solve this issue

Thanks

ラベル(6)
0 件の賞賛
返信
3 返答(返信)

588件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi charles

this link also mentions the same kernel patch for wandboard imx_3.10.17_1.0.0_ga

ASoC: sgtl5000: Fix the cache handling · wandboard-org/linux@55d6dfb · GitHub

Best regards

igor

0 件の賞賛
返信

588件の閲覧回数
charleshuang
Senior Contributor II

Hi

I try your patch,but I got kernel panic after playing music and reset my device

Attached is kernel message

thanks

0 件の賞賛
返信

588件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

you are using customized advantech linux, so it may be

recommended to apply to them for modifications.

Alternatively one can debug it using AN4553

Using Open Source Debugging Tools for Linux on i.MX Processors

~igor

0 件の賞賛
返信