when I use "repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-gatesgarth -m imx-5.10.9-1.0.0.xml " to download imx6qsabresd project. then an error occurred."ERROR: gstreamer1.0-1.14.4.imx-r0 do_fetch: Fetcher failure for URL: 'gitsm://source.codeaurora.org/external/imx/gstreamer.git;protocol=https;branch=MM_04.05.02_1911_L4.14.98'. Unable to fetch URL from any source." How can I correct the GStreamer download method?
thanks
fetch error is network issue, I suggest that you delete the package and bitbake again
I can delete under ~/fsl-release-bsp/build-x11/tmp/work$ about gstreamer path. not download gstreamer . later I can delter under ~/fsl-release-bsp/build-x11/tmp/work$ and under ~/fsl-release-bsp/sources
about gstreamer path. but I cann't l download gstreamer
use bitbake -c cleansstate xxx to clean package, then use bitbake to build again