X does not support your locale
libpng warning: iCCP: known incorrect sRGB profile
libpng warning: iCCP: cHRM chunk does not match sRGB
X11 Error encountered:
Error: BadMatch (invalid parameter attributes)
Request: 1 (0)
Resource ID: 0x1600082
Serial: 2228
Hwnd: Hwnd, Mapped:False ClientWindow:0x1600083, WholeWindow:0x1600082, Zombie=False, Parent:[Hwnd, Mapped:False ClientWindow:0x1600011, WholeWindow:0x1600010, Zombie=False, Parent:[<null>]]
Control: <handle 1600083 non-existant> at System.Environment.get_StackTrace () [0x00000] in <99b7767fda36428caf8c4eed0d54aaec>:0
I have attached board and xorg.o.log
Hi Bio_TICFSL
I changed kernel to 4.19
BUILD
BB_VERSION = "1.42.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "ubuntu-16.04"
TARGET_SYS = "arm-poky-linux-gnueabi"
MACHINE = "imx6ull9x9evk"
DISTRO = "fsl-imx-x11"
DISTRO_VERSION = "4.19-warrior"
Initially I was getting
System.NotSupportedException: [X11] GLX extension is not supported.
which got solved by adding the following lines in conf/local.conf
IMAGE_INSTALL_append = " xserver-xorg xserver-xorg-extension-glx "
DISTRO_FEATURES_append = " systemd opentk glx "
Still i am getting the same error also i have attached Xorg.0.log for your reference
Hello sheraz,
Which BSP are you using? since in the latest BSP this error is fixed, however is correspond to X11, not from the backend, please check the web site.
Regards
Hi Bio_TICFSL
I am using imx6ull with linux kernel version
$uname -a
Linux iWave-G18M 4.1.15 #1 SMP PREEMPT Thu Jul 19 17:37:39 IST 2018 armv7l armv7l armv7l GNU/Linux
What changes need to be done to remove x11 error
Thanks and Regards
Sheraz Ali Shah
DISTRO = "poky"
DISTRO_NAME = "Poky (Yocto Project Reference Distro)"
DISTRO_VERSION = "2.1.1"
DISTRO_CODENAME = "krogoth"
SDK_VENDOR = "-pokysdk"
SDK_VERSION := "${@'${DISTRO_VERSION}'.replace('snapshot-${DATE}','snapshot')}"
FILE :- sources/poky/meta-poky/conf/distro/poky.conf
I am using krogoth branch