Dear All :
I want to use CentOS 64 install ltib and build U-boot .
But I only find this document use CentOS
CentOS 6.3 64-bit Host Building i.MX6Q-SDB Linux L3.0.35_12.09.01.01_GA_Source
so I think ,if I want to use CentOS build code and I have to use L3.0.35_12.09.01?
Because I try to use L3.0.35_4.1.0_130816_source code , it's can't work.
please give me some idea!!!
已解决! 转到解答。
I think it would be better to use Ubuntu or Debian as host PC for
i.MX6 Linux building, since this Linux branch mainly is used by BSP
designers.
Please refer to the next Community link for recent
recommendations about Linux host setup :
"i.MX Linux BSP Environment Setup"
https://community.freescale.com/docs/DOC-95042
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
I think it would be better to use Ubuntu or Debian as host PC for
i.MX6 Linux building, since this Linux branch mainly is used by BSP
designers.
Please refer to the next Community link for recent
recommendations about Linux host setup :
"i.MX Linux BSP Environment Setup"
https://community.freescale.com/docs/DOC-95042
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------