Hi the imx6d/Q supports two parallel and one mipi camera interface.We want to utilise them for the video specific application.We want to record threee full HD (1080P) camera inputs and store it in the SDXC memory.Also the the three videos shall be displayed on the HDMI screen.
Wheter imx6D/Q can support this application Please clarify.
The camere spec is as bleow
1 | Compression Method | H.264 |
2 | Firm rate | ~30FPS |
3 | Bit rate | ~20Mbps( |
4 | Bit rate control | CBR(Fixed Bit rate) |
5 | Video Resolution | 1920 × 1080(Maximum) |
6 | Encryption | I Picture Encryption |
7 | OSD Display Video output side | Status Display (Recording, Idle state, GNSS position status) |
8 | OSD Display Video input side | Time Display, CH Display |
Please provide your inputs.
Best Regards
Saleem