wake up from usb(i.MX6)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

wake up from usb(i.MX6)

1,150 次查看
hyunhoshin
Contributor III

I want to use USB type LTE Dongle on i.MX6

I wonder if i.MX6 can wake up via USB LTE modem when it is in sleep mode.

标签 (1)
标记 (3)
0 项奖励
1 回复

935 次查看
igorpadykov
NXP Employee
NXP Employee

Hi hyunho

yes i.MX6 can wake up via USB, for usage one can follow sect.39.2.4 USB Wakeup Usage

attached Linux Guide.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励