wake up from usb(i.MX6)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

wake up from usb(i.MX6)

1,151件の閲覧回数
hyunhoshin
Contributor III

I want to use USB type LTE Dongle on i.MX6

I wonder if i.MX6 can wake up via USB LTE modem when it is in sleep mode.

ラベル(1)
タグ(3)
0 件の賞賛
1 返信

936件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi hyunho

yes i.MX6 can wake up via USB, for usage one can follow sect.39.2.4 USB Wakeup Usage

attached Linux Guide.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛