valid dts files for Sabre Lite board with kernel 3.10.53

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

valid dts files for Sabre Lite board with kernel 3.10.53

1,820 Views
dmitryfedotov
Contributor II

Hello, All

Where can I find valid imx6q-sabrelite.dts file with framebuffer support. In exist official kernel git repository(imx_3.10.53_1.1.0_ga branch) linux started normally with COM-console, but not found any HDMI devices.

BR.

Labels (2)
0 Kudos
Reply
7 Replies

1,243 Views
EricNelson
Senior Contributor II

Hi Dmitry,

I'm not sure if you caught this, but we've released 3.10.53:

     http://boundarydevices.com/i-mx6-kernel-3-10-53/

0 Kudos
Reply

1,243 Views
OtavioSalvador
Senior Contributor II

Just as a heads up, it is now merged in FSL Community BSP Fido branch.         

0 Kudos
Reply

1,243 Views
EricNelson
Senior Contributor II

Hello Dmitry,

The imx_3.10.53_1.1.0_ga branch just dropped yesterday, so you'll need to give us a week or so to get things ported for SABRE Lite.


We have a full-featured set for 3.10.31_1.1.0_beta, and it's likely that the device tree is close, but it will take a while to do

regression testing against Freescale's new code base.

     boundarydevices/linux-imx6 at boundary-imx_3.10.31_1.1.0_beta · GitHub

0 Kudos
Reply

1,243 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi Eric,

I wonder if the porting to the SABRE Lite is done.

Thanks a lot,

Alejandro

0 Kudos
Reply

1,243 Views
EricNelson
Senior Contributor II

Hi Alejandro,

Unfortunately, not yet. The port from 3.10.31 to 3.10.53 is a bit bigger than expected.

0 Kudos
Reply

1,243 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi Eric,

Thanks a lot. It would be aprreciated if you keep us informed.

Best Regards,

Alejandro

0 Kudos
Reply

1,243 Views
EricNelson
Senior Contributor II

Hi Alejandro,

This is still very much a work in progress. The LVDS display support is quite different and we haven't yet figured out a way to handle all of our displays in a graceful manner.

If you want to take a look at some preliminary work, you can check in our "boundary-imx_3.10.53_1.1.0_ga-pass1" branch.

0 Kudos
Reply