Hello, All
Where can I find valid imx6q-sabrelite.dts file with framebuffer support. In exist official kernel git repository(imx_3.10.53_1.1.0_ga branch) linux started normally with COM-console, but not found any HDMI devices.
BR.
Hi Dmitry,
I'm not sure if you caught this, but we've released 3.10.53:
Just as a heads up, it is now merged in FSL Community BSP Fido branch.
Hello Dmitry,
The imx_3.10.53_1.1.0_ga branch just dropped yesterday, so you'll need to give us a week or so to get things ported for SABRE Lite.
We have a full-featured set for 3.10.31_1.1.0_beta, and it's likely that the device tree is close, but it will take a while to do
regression testing against Freescale's new code base.
boundarydevices/linux-imx6 at boundary-imx_3.10.31_1.1.0_beta · GitHub
Hi Eric,
I wonder if the porting to the SABRE Lite is done.
Thanks a lot,
Alejandro
Hi Alejandro,
Unfortunately, not yet. The port from 3.10.31 to 3.10.53 is a bit bigger than expected.
Hi Eric,
Thanks a lot. It would be aprreciated if you keep us informed.
Best Regards,
Alejandro
Hi Alejandro,
This is still very much a work in progress. The LVDS display support is quite different and we haven't yet figured out a way to handle all of our displays in a graceful manner.
If you want to take a look at some preliminary work, you can check in our "boundary-imx_3.10.53_1.1.0_ga-pass1" branch.