uboot201603 hangs on Uncompressing Linux... done, booting the kernel

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

uboot201603 hangs on Uncompressing Linux... done, booting the kernel

932 次查看
末班车上的乘客
Contributor II

uboot201603 boot zImage(4.1.15) hangs on Uncompressing Linux... done, booting the kernel.it's print error message occasionally,seems it's crashed at clk_mux_get_parent().I‘ll paste log later

174945_174945.jpgIMG_20170123_112414R.jpg

zImage boots okay with uboot201404

my board file config

 

static iomux_v3_cfg_t const uart1_pads[] = {
MX6_PAD_SD3_DAT7__UART1_TX_DATA | MUX_PAD_CTRL(UART_PAD_CTRL),
MX6_PAD_SD3_DAT6__UART1_RX_DATA | MUX_PAD_CTRL(UART_PAD_CTRL),
};

 

static iomux_v3_cfg_t const usdhc1_pads[] = {
MX6_PAD_SD1_CMD__SD1_CMD | MUX_PAD_CTRL(USDHC_PAD_CTRL),
MX6_PAD_SD1_CLK__SD1_CLK | MUX_PAD_CTRL(USDHC_PAD_CTRL),
MX6_PAD_SD1_DAT0__SD1_DATA0 | MUX_PAD_CTRL(USDHC_PAD_CTRL),
MX6_PAD_SD1_DAT1__SD1_DATA1 | MUX_PAD_CTRL(USDHC_PAD_CTRL),
MX6_PAD_SD1_DAT2__SD1_DATA2 | MUX_PAD_CTRL(USDHC_PAD_CTRL),
MX6_PAD_SD1_DAT3__SD1_DATA3 | MUX_PAD_CTRL(USDHC_PAD_CTRL),
//MX6_PAD_EIM_D16__GPIO3_IO16 | MUX_PAD_CTRL(NO_PAD_CTRL), /* SD1_CD for eq6708 */
MX6_PAD_EIM_D17__GPIO3_IO17 | MUX_PAD_CTRL(NO_PAD_CTRL), /* SD1_CD for epc6708 */
MX6_PAD_EIM_D18__GPIO3_IO18 | MUX_PAD_CTRL(NO_PAD_CTRL), /* WP */
};

static iomux_v3_cfg_t const usdhc3_pads[] = {
MX6_PAD_SD3_CLK__SD3_CLK | MUX_PAD_CTRL(USDHC_PAD_CTRL),
MX6_PAD_SD3_CMD__SD3_CMD | MUX_PAD_CTRL(USDHC_PAD_CTRL),
MX6_PAD_SD3_DAT0__SD3_DATA0 | MUX_PAD_CTRL(USDHC_PAD_CTRL),
MX6_PAD_SD3_DAT1__SD3_DATA1 | MUX_PAD_CTRL(USDHC_PAD_CTRL),
MX6_PAD_SD3_DAT2__SD3_DATA2 | MUX_PAD_CTRL(USDHC_PAD_CTRL),
MX6_PAD_SD3_DAT3__SD3_DATA3 | MUX_PAD_CTRL(USDHC_PAD_CTRL),
MX6_PAD_GPIO_17__GPIO7_IO12 | MUX_PAD_CTRL(NO_PAD_CTRL), /* CD */
MX6_PAD_GPIO_18__GPIO7_IO13 | MUX_PAD_CTRL(NO_PAD_CTRL), /* WP */
};

static iomux_v3_cfg_t const usdhc4_pads[] = {
MX6_PAD_SD4_CLK__SD4_CLK | MUX_PAD_CTRL(USDHC_PAD_CTRL),
MX6_PAD_SD4_CMD__SD4_CMD | MUX_PAD_CTRL(USDHC_PAD_CTRL),
MX6_PAD_SD4_DAT0__SD4_DATA0 | MUX_PAD_CTRL(USDHC_PAD_CTRL),
MX6_PAD_SD4_DAT1__SD4_DATA1 | MUX_PAD_CTRL(USDHC_PAD_CTRL),
MX6_PAD_SD4_DAT2__SD4_DATA2 | MUX_PAD_CTRL(USDHC_PAD_CTRL),
MX6_PAD_SD4_DAT3__SD4_DATA3 | MUX_PAD_CTRL(USDHC_PAD_CTRL),
MX6_PAD_SD4_DAT4__SD4_DATA4 | MUX_PAD_CTRL(USDHC_PAD_CTRL),
MX6_PAD_SD4_DAT5__SD4_DATA5 | MUX_PAD_CTRL(USDHC_PAD_CTRL),
MX6_PAD_SD4_DAT6__SD4_DATA6 | MUX_PAD_CTRL(USDHC_PAD_CTRL),
MX6_PAD_SD4_DAT7__SD4_DATA7 | MUX_PAD_CTRL(USDHC_PAD_CTRL),
};

 

struct fsl_esdhc_cfg usdhc_cfg[2] = {
// {USDHC1_BASE_ADDR},
{USDHC3_BASE_ADDR},
{USDHC4_BASE_ADDR},
};

/*#define USDHC1_CD_GPIO IMX_GPIO_NR(3, 16) */ /* for eq6708*/
#define USDHC1_CD_GPIO IMX_GPIO_NR(3, 17) /* for epc6708*/
#define USDHC3_CD_GPIO IMX_GPIO_NR(7, 12)

int board_mmc_get_env_dev(int devno)
{
return devno - 2;
}

int mmc_map_to_kernel_blk(int devno)
{
return devno + 2;
}

int board_mmc_getcd(struct mmc *mmc)
{
struct fsl_esdhc_cfg *cfg = (struct fsl_esdhc_cfg *)mmc->priv;
int ret = 0;

switch (cfg->esdhc_base) {
/* case USDHC1_BASE_ADDR:
ret = !gpio_get_value(USDHC1_CD_GPIO);
break;*/
case USDHC3_BASE_ADDR:
ret = !gpio_get_value(USDHC3_CD_GPIO);
break;
case USDHC4_BASE_ADDR:
ret = 1; /* eMMC/uSDHC4 is always present */
break;
}

return ret;
}

int board_mmc_init(bd_t *bis)
{
int ret;
int i;

/*
* According to the board_mmc_init() the following map is done:
* (U-Boot device node) (Physical Port)
* mmc0 SD1
* mmc1 SD3
* mmc2 eMMC
*/
for (i = 0; i < CONFIG_SYS_FSL_USDHC_NUM; i++) {
switch (i) {
/* case 0:
imx_iomux_v3_setup_multiple_pads(
usdhc1_pads, ARRAY_SIZE(usdhc1_pads));
gpio_direction_input(USDHC1_CD_GPIO);
usdhc_cfg[0].sdhc_clk = mxc_get_clock(MXC_ESDHC_CLK);
usdhc_cfg[0].max_bus_width = 4;
break;*/
case 0:
imx_iomux_v3_setup_multiple_pads(
usdhc3_pads, ARRAY_SIZE(usdhc3_pads));
gpio_direction_input(USDHC3_CD_GPIO);
usdhc_cfg[0].sdhc_clk = mxc_get_clock(MXC_ESDHC3_CLK);
usdhc_cfg[0].max_bus_width = 4;
break;
case 1:
imx_iomux_v3_setup_multiple_pads(
usdhc4_pads, ARRAY_SIZE(usdhc4_pads));
usdhc_cfg[1].sdhc_clk = mxc_get_clock(MXC_ESDHC4_CLK);
break;
default:
printf("Warning: you configured more USDHC controllers"
"(%d) then supported by the board (%d)\n",
i + 1, CONFIG_SYS_FSL_USDHC_NUM);
return -EINVAL;
}

ret = fsl_esdhc_initialize(bis, &usdhc_cfg[i]);
if (ret)
return ret;
}

return 0;
}

 

my environment configs

 

#define CONFIG_EXTRA_ENV_SETTINGS \
CONFIG_MFG_ENV_SETTINGS \
"fdt_addr=0x18000000\0" \
"fdt_high=0xffffffff\0" \
"bootargs_base=console=" CONFIG_CONSOLE_DEV ",115200 \0" \
"mmcdev="__stringify(CONFIG_SYS_MMC_ENV_DEV)"\0" \
"mmcpart=" __stringify(CONFIG_SYS_MMC_ENV_PART) "\0" \
"mmcroot=" CONFIG_MMCROOT " rootwait rw\0" \
"serverip=" CONFIG_SERVERIP "\0" \
"ipaddr=" CONFIG_IPADDR "\0" \
"ethaddr=00:00:00:00:00:03\0" \
"nfsroot=/home/jiajizhong/nfsdir\0" \
"u-boot=u-boot.imx\0" \
"kernel=zImage\0" \
"loglevel=1\0" \
"splashimage=0x17a00000\0" \
"bmp_file=logo.bmp\0" \
"fec_mode=rgmii\0" \
"adv7611=enable\0" \
"ldb0_panel=dev=ldb,if=RGB24 ldb=sin0\0" \
"ldb1_panel=dev=ldb,if=RGB24 ldb=sin1\0" \
"ldbdul_panel=dev=ldb,if=RGB24 ldb=dul1\0" \
"hdmi_panel=dev=hdmi,1920x1080M@60,if=RGB24\0" \
"lcd_panel=dev=lcd,SEIKO-WVGA,if=RGB24\0" \
"pridis=mxcfb0:dev=ldb,if=RGB24 ldb=sin1\0" \
"secdis=mxcfb1:dev=lcd,SEIKO-WVGA,if=RGB24\0" \
"fdt_file=imx6dl-" CONFIG_BOARD_NAME ".dtb\0" \
"loadimage=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${kernel}\0" \
"loadfdt=fatload mmc ${mmcdev}:${mmcpart} ${fdt_addr} ${fdt_file}\0" \
"bootargs_mmc=setenv bootargs; setenv bootargs ${bootargs_base} root=${mmcroot} "\
"video=${pridis} video=${secdis} loglevel=${loglevel} earlyprintk\0" \
"bootcmd_mmc=run bootargs_mmc; run loadimage; run loadfdt; " \
"bootz ${loadaddr} - ${fdt_addr} \0" \
"bootcmd_tftp=run bootargs_mmc; "\
"tftpboot ${loadaddr} ${kernel}; " \
"tftpboot ${fdt_addr} ${fdt_file}; " \
"bootz ${loadaddr} - ${fdt_addr} \0" \
"bootargs_nfs=setenv bootargs; setenv bootargs ${bootargs_base} " \
"root=/dev/nfs ip=${ipaddr} nfsroot=${serverip}:${nfsroot},v3,tcp\0" \
"bootcmd_nfs=run bootargs_nfs; " \
"tftpboot ${loadaddr} ${kernel}; " \
"tftpboot ${fdt_addr} ${fdt_file}; " \
"bootz ${loadaddr} - ${fdt_addr}\0" \
"bootargs_mem=setenv bootargs; setenv bootargs ${bootargs_base} " \
"rdinit=/etc/inittab enable_wait_mode=off \0" \
"bootcmd_mem=run bootargs_mem; " \
"tftpboot ${loadaddr} uImage.ramdisk; " \
"tftpboot ${fdt_addr} rootfs.ramdisk; " \
"bootm ${loadaddr} ${fdt_addr}\0" \
"update_uboot=tftpboot ${loadaddr} ${u-boot};" \
"sf probe; sf erase 0 0x200000;" \
"sf write ${loadaddr} 0x400 0x80000\0" \
"bootcmd=run bootcmd_mmc \0"
#endif

Original Attachment has been moved to: mx6eq6708_common.h.zip

Original Attachment has been moved to: mx6eq6708.h.zip

Original Attachment has been moved to: mx6eq6708.c.zip

Original Attachment has been moved to: mx6eq6708android_common.h.zip

标签 (3)
0 项奖励
回复
1 回复

666 次查看
igorpadykov
NXP Employee
NXP Employee

Hi

had you tried ddr test for board

https://community.freescale.com/docs/DOC-105652 

and rebuilt uboot with new calibration coefficients in

uboot../board_name/*.cfg file.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复