Hi
I take below article as reference for support tw9992 blending mode, and refer attachment ISL79987&adv7180_reference_driver_for_iMX8QXP.7z
ISL79987 and adv7180 de-interlace driver for iMX8QXP boards
In my case, camera links to isi0, TV links to isi4
The TV weaving mode is OK.
But TV blending mode is fail
This is blending mode setting in dts file
Does anyone has suggestion?
Thanks
&i2c0_mipi_csi1 {
clock-frequency = <100000>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_mipi_csi1_i2c0>;
status = "okay";
tw9992_mipi:tw9992_mipi@44 {
compatible = "renesas,tw9992_mipi";
reg = <0x44>;
pinctrl-names = "default";
/* pinctrl-0 = <&pinctrl_mipi_csi1>; */
pinctrl-0 = <&pinctrl_mipi_csi1_en_rst>;
clocks = <&clk IMX8QM_24MHZ>;
clock-names = "csi_mclk";
csi_id = <1>;
rst-gpios = <&gpio1 30 GPIO_ACTIVE_LOW>;
video1en_gpio = <&gpio2 30 GPIO_ACTIVE_LOW>;
digtr2_gpio = <&gpio0 1 GPIO_ACTIVE_HIGH>;
digo2_gpio = <&gpio0 2 GPIO_ACTIVE_LOW>;
video2en_gpio = <&gpio2 31 GPIO_ACTIVE_LOW>;
digtr3_gpio = <&gpio2 17 GPIO_ACTIVE_HIGH>;
digo3_gpio = <&gpio0 16 GPIO_ACTIVE_LOW>;
mclk = <27000000>;
mclk_source = <0>;
mipi_csi;
status = "okay";
port {
tw9992_mipi_ep: endpoint {
remote-endpoint = <&mipi_csi1_ep>;
};
};
};
};
&mipi_csi_1 {
/delete-property/virtual-channel;
status = "okay";
port@1 {
reg = <1>;
mipi_csi1_ep: endpoint {
remote-endpoint = <&tw9992_mipi_ep>;
data-lanes = <1 2>;
};
};
};
&isi_4 {
interface = <3 0 2>;
deinterlace_mode = <4>;
/* 0 ~ 1: No de-interlacing,
2: Odd even weave, 3: Even odd weave
4: Odd even blending, 5: Even odd blending
6 ~ 7: Line doubling */
deinterlace_blending;
status = "okay";
};
Hi Simon
reason may be ISI errata since i.MX8QM has similar ISI errata as iMX8QXP B0.
As described on article:
"blending mode de-interlace can only work on iMX8QXP C0 chips"
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igorpadykov
I check p.7224 in iMX8QM_RM_Rev_F.pdf
It support blend de-interlace mode
System always repeat below log and doesn't display preview after I set blending mode
[ 85.771754] ---> mxc_isi_capture_open
[ 85.775474] ---> mxc_isi_get_remote_source_pad
[ 85.780220] ---> mxc_isi_cap_querycap
[ 85.784005] ---> mxc_isi_cap_g_chip_ident
[ 85.790170] ---> mxc_isi_get_remote_source_pad
[ 85.800440] ---> mxc_isi_capture_release
[ 85.804746] ---> mxc_isi_get_remote_source_pad
This is my current dts file
&isi_4 {
deinterlace_mode = <5>;
/* 0 ~ 1: No de-interlacing,
2: Odd even weave, for PAL
3: Even odd weave, for NTSC
4: Odd even blending, for PAL
5: Even odd blending, for NTSC
6 ~ 7: Line doubling */
deinterlace_blending;
ntsc_top = <0>;
status = "okay";
}
Do you have any suggestion?
Thanks