Hi xin wang,
It's *.dts file, not *.c. In the yocto it use the device tree structure.
Have a nice day
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi xin wang,
The path is root/arch/arm/boot/dts/imx6q-sabresd.dts. You can check the path in your source code.
linux-2.6-imx.git - Freescale i.MX Linux Tree
Have a nice day
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Dan Wang,
Thanks for reply.
I have checked the *.dts file, it seems like a configuration for chip resource, but i need the C source file, like "Board-mx6q_sabresd.c", which Implements the board initial API (like "mx6_sabresd_board_init"), the uart initial API (like "mx6q_sabresd_init_uart"), etc.
Thanks a lot. : )
Hi xin wang,
It's *.dts file, not *.c. In the yocto it use the device tree structure.
Have a nice day
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi xin wang,
You're welcome. It's my pleasure:smileyhappy:. You can read and refer to the Freescale_Yocto_Project_User's_Guide.pdf provide in our website. And the Yocto training also can help you, Yocto Training - HOME If you have new questions you can create new threads in our community.
Have a nice day and weekend
Dan