supporting Gigabit Ethernet in imx6 board by yocto L4.1.15

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

supporting Gigabit Ethernet in imx6 board by yocto L4.1.15

787 次查看
qi908542785
Contributor I

Hi,

We are using a Sabresd board (i.MX6Q) with YOCTO 4.1.15 kernel.On the basis of Sabresd board own development board.

The system default is 100M Ethernet,We want to achieve Gigabit Ethernet.

What need to modify the support Gigabit Ethernet,Hope to get your help.

Regards,

QI.

0 项奖励
回复
1 回复

466 次查看
igorpadykov
NXP Employee
NXP Employee

Hi

please check rgmii timing with oscilloscope given in

Table 62. RGMII Signal Switching Specifications i.MX6DQ Datasheet

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复