supporting Gigabit Ethernet in imx6 board by yocto L4.1.15

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

supporting Gigabit Ethernet in imx6 board by yocto L4.1.15

770件の閲覧回数
qi908542785
Contributor I

Hi,

We are using a Sabresd board (i.MX6Q) with YOCTO 4.1.15 kernel.On the basis of Sabresd board own development board.

The system default is 100M Ethernet,We want to achieve Gigabit Ethernet.

What need to modify the support Gigabit Ethernet,Hope to get your help.

Regards,

QI.

0 件の賞賛
返信
1 返信

449件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi

please check rgmii timing with oscilloscope given in

Table 62. RGMII Signal Switching Specifications i.MX6DQ Datasheet

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信