substitution of Ethernet phy chip

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

substitution of Ethernet phy chip

1,741 Views
kilsuhong
Contributor I

Dear,

I have tried to change ethernet phy chip (AR8031 --> Realtek 8211).

I added phy driver structure as below

====================================================================

.phy_id = 0x001cc912,

.name  = "RTL8211B Gigabit Ethernet",

.phy_id_mask = 0x001fffff,

.features  = PHY_GBIT_FEATURES,

.flags  = PHY_HAS_INTERRUPT,

.config_aneg = &genphy_config_aneg,

.read_status  = &genphy_read_status,

.ack_interrupt = &rtl821x_ack_interrupt,

.config_intr  = &rtl8211b_config_intr,

.driver  = { .owner = THIS_MODULE,},

====================================================================


But, my device cannot find eth0.

I looked through source code, and at "fec_enet_mii_probe", there is no phy_map information


=====================================================================

static int fec_enet_mii_probe(struct net_device *ndev)

{

  struct fec_enet_private *fep = netdev_priv(ndev);

  struct phy_device *phy_dev = NULL;

  char mdio_bus_id[MII_BUS_ID_SIZE];

  char phy_name[MII_BUS_ID_SIZE + 3];

  int phy_id;

  int dev_id = fep->pdev->id;

  fep->phy_dev = NULL;

  /* check for attached phy */

  for (phy_id = 0; (phy_id < PHY_MAX_ADDR); phy_id++) {

       if ((fep->mii_bus->phy_mask & (1 << phy_id)))

            continue;

       if (fep->mii_bus->phy_map[phy_id] == NULL)

            continue;

       if (fep->mii_bus->phy_map[phy_id]->phy_id == 0)

             continue;

       if (dev_id--)

            continue;

       strncpy(mdio_bus_id, fep->mii_bus->id, MII_BUS_ID_SIZE);

       break;

  }

.......

=====================================================================


what should I check to register phy_map?

In addition, where can I find AR8031 driver source code and how register information for AR8031 to platform?

(My base source code is mx6dl_sabreSD)


Labels (3)
0 Kudos
1 Reply

810 Views
igorpadykov
NXP Employee
NXP Employee

Hi kilsu

recommended to check with oscilloscope clock and data signals

and check them with datasheet, also below links gives descriptions

of possible issues with new phy

Using RGMII compatible PHY with i.MX6 (u-boot)

iMX6q RGMII back to back connection with FPGA

https://community.freescale.com/thread/289362

for ethernet sources one can look at attached linux manual

sect.44.2.2 Source Code Structure

Also AR8031 settings may be not fully compatible with

Realtek 8211, suggest to ask realtek support for driver for this chip.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------