ChuYuan Chiang asked4 days ago
Hi,
I found this url Porting WM8960 to Android jb4.2.2 about porting the wm8960 in android (kernel version is 3.0.35)
but in yocto 1.6.2 that is using device tree and 3.10.53 kernel.
I try port it, but the AUD3_TXD still not output any signal.
the following is my device tree for sound part:
sound { | |||
compatible = "fsl,imx-audio-wm8960"; | |||
model = "wm8960-audio"; | |||
cpu-dai = <&ssi2>; | |||
audio-codec = <&codec>; | |||
codec-master; | |||
gpr = <&gpr>; | |||
audio-routing = | |||
"Headset Jack", "HP_L", | |||
"Headset Jack", "HP_R", | |||
"Ext Spk", "SPK_LP", | |||
"Ext Spk", "SPK_LN", | |||
"Ext Spk", "SPK_RP", | |||
"Ext Spk", "SPK_RN"; | |||
hp-det = <3 1>; | |||
hp-det-gpios = <&gpio7 8 0>; | |||
mic-det-gpios = <&gpio1 9 0>; | |||
}; |
codec: wm8960@1a { | ||
compatible = "wlf,wm8960"; | ||
reg = <0x1a>; | ||
status = "okay"; | ||
clocks = <&clks 201>; | ||
clock-names = "mclk"; | ||
wlf,shared-lrclk; |
};
&audmux {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_audmux_wcp>;
status = "okay";
ssi2 {
fsl,audmux-port = <MX31_AUDMUX_PORT2_SSI1>;
fsl,port-config = <
(IMX_AUDMUX_V2_PTCR_TFSDIR |
IMX_AUDMUX_V2_PTCR_SYN |
IMX_AUDMUX_V2_PTCR_TFSEL(MX31_AUDMUX_PORT3_SSI_PINS_3) |
IMX_AUDMUX_V2_PTCR_TCLKDIR |
IMX_AUDMUX_V2_PTCR_TCSEL(MX31_AUDMUX_PORT3_SSI_PINS_3))
IMX_AUDMUX_V2_PDCR_RXDSEL(MX31_AUDMUX_PORT3_SSI_PINS_3)
>;
};
aud3 {
fsl,audmux-port = <MX31_AUDMUX_PORT3_SSI_PINS_3>;
fsl,port-config = <
IMX_AUDMUX_V2_PTCR_SYN
IMX_AUDMUX_V2_PDCR_RXDSEL(MX31_AUDMUX_PORT2_SSI1)
>;
};
};
Dose any one have idea about this?
Thanks,
ChuYuan
Hello,
Please check carefully Your configuration using Chapter 8 (Porting Audio Codecs
to a Custom Board) of “i.MX_6_BSP_Porting_Guide.pdf” in Linux BSP documentation
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX6_SW
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------