sitronix-st7701 panel issue with kernel 5.15.71 (kirkstone)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

sitronix-st7701 panel issue with kernel 5.15.71 (kirkstone)

1,439 Views
kishan_dudhatra
Contributor III

Hi folks;
@Zhiming_Liu 

I am trying to bring up sitronix-st7701 display panel in imx8mm. This display panel is working on yocto zeus. I have ported the same driver in kirkstone. during boot time, we get the Linux logo means the display driver is working. After the boot, I am getting the below error and the display goes off.

[   14.046955] imx_sec_dsim_drv 32e10000.mipi_dsi: wait rx done time out
[   14.430905] imx_sec_dsim_drv 32e10000.mipi_dsi: wait payload tx done time out

 But after restarting Weston service display works.

Anyone can suggest where to debug?

Regards,
Kishan Dudhatra
0 Kudos
Reply
5 Replies

1,415 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport
0 Kudos
Reply

1,403 Views
kishan_dudhatra
Contributor III

Hi @Bio_TICFSL 

Thanks for the quick reply.

I have read this thread https://community.nxp.com/t5/i-MX-Processors/how-to-add-a-new-panel-with-imx8mm-evk-I-got-some-probl...  but unable to get the solutions for the below error logs.

[   14.046955] imx_sec_dsim_drv 32e10000.mipi_dsi: wait rx done time out
[   14.430905] imx_sec_dsim_drv 32e10000.mipi_dsi: wait payload tx done time out

As previously I mentioned this display is working on Zeus kernel 4.9 but goes off on Kirkstone kernel 5.15.71 after booting and need to restart the Weston services. We also got the Linux logo on display during the boot which means the display driver is working. After restarting the Weston service display is working. Can you please provide suggestions on mentioned error logs?

Thanks in advance. 

Regards,
Kishan Dudhatra
0 Kudos
Reply

1,358 Views
kishan_dudhatra
Contributor III

Hi @Bio_TICFSL ,

Can you please provide suggestions for the issue?

Regards,
Kishan Dudhatra
0 Kudos
Reply

1,178 Views
Udhay_
Contributor III

@kishan_dudhatra 

did you resolve this?

 

Tags (1)
0 Kudos
Reply

1,126 Views
kishan_dudhatra
Contributor III
@Udhay_
systemd-backlight@.service was causing issues, so I removed the service.

Regards,
Kishan Dudhatra
0 Kudos
Reply