second ethernet port do not work arfter suddenly power down

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

second ethernet port do not work arfter suddenly power down

816 Views
cyndent
Contributor I

i have both 6ul/6ull board and they all have two etherent port using lan8720a phy.

linux kernel i have tried 4.15/4.4.

After warm reboot, the second ethernet port works well.

But after cold reboot,the second ethernet port do not work

i have known that it's a power-on sequence problem.But i'm a beginner of linux,i do not know what to do next.

Can someone tell me how to check about it?

Thanks!

Labels (2)
0 Kudos
Reply
2 Replies

666 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Mingyang,

The table Reset Priorities, Sources, Types, and Behavior from user's manual used by ALU. It shows the reset propagation to IP bloc. There is 3 warm reset depending of sources ( see below ). I guess that the one connected to ENET is system_rst_b because it drives functional modules. Based on table below, it means that ENET isn't reseted. The is also an other useful drawing on Reset Diagram.

Table 59-2. Reset Priorities, Sources, Types, and Behavior.jpgRegards

0 Kudos
Reply

666 Views
cyndent
Contributor I

Hi Bio_TICFSL:

   Sorry for the late reply. I have check the document and find the difference as you say above.

   But i'm still confusing about the process that when does it work and how can i fix it? Is it working in kernel or uboot? or just in chips that i can not modify it? or i have make some modifies in hardware? 

   i have searched in kernel and uboot but i have find nothing about system_rst_b.

   Can you give some advices about that? Thanks very much.

0 Kudos
Reply