I am building the ota file for imx6 platform in Marshmallow. i obtained the ota zip file but it doesn't have new images, I am getting update in META data file only. I am not getting updated Boot.img and system.img
I had followed the below steps to get OTA File
make otapackage
make PRODUCT=sabresd_6dq-eng otapackage -j4
Then zip file is created with compiled date by using ls -l command
->sabresd_6dq-ota-20160331-imx6q.zip
After unzip, ls -l command result as follows,
-rw-rw-r-- 1 zumi-02 zumi-02 8865064 Jul 14 2011 boot.img
-rw-rw-r-- 1 zumi-02 zumi-02 445440 Jul 14 2011 bootloader.img
-rw-rw-r-- 1 zumi-02 zumi-02 15407 Jul 14 2011 file_contexts
-rw-r--r-- 1 zumi-02 zumi-02 271684670 May 22 20:21 sabresd_6dq-ota-20160331-imx6q.zip
-rw-rw-r-- 1 zumi-02 zumi-02 536703003 Jul 14 2011 system.new.dat
-rw-rw-r-- 1 zumi-02 zumi-02 0 Jul 14 2011 system.patch.dat
-rw-rw-r-- 1 zumi-02 zumi-02 345 Jul 14 2011 system.transfer.list
Can anyone help me to resolve this issue to get updated Images.
Hi Rita,
Bsp i am using is android 6.0.1.
Hi Rita,
Thanks first of all
i done the following command
make dist
but no update in zip file
ritayang i am attaching the test case for "signature failed" in reboot recovery .
i am attaching the log of the failure in the below file.
Supported API: 3
Finding update package...
I:Update location: /cache/sabresd_6dq-ota-20160331.zip
Opening update package...
I:read key e=3 hash=20
I:1 key(s) loaded from /res/keys
Verifying update package...
I:comment is 1746 bytes; signature 1728 bytes from end
I:failed to verify against RSA key 0
E:failed to verify whole-file signature
I:verify_file returned 1
E:signature verification failed
Installation aborted.
I:timed out waiting for key input; rebooting.
Hi,
Please read the attachment file, it will help you.
Have a great day,
Rita
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
You can refer to the follow threads, hope these can do help for you.
Verification OTA w/ update.zip and diff-ota.zip
iMX6q sabersd OTA update
Have a great day,
Rita
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
Which version BSP are you using?
Have a nice day
Rita