sabresd_6dq-ota-20160331-imx6q.zip NOT Having new images inside ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

sabresd_6dq-ota-20160331-imx6q.zip NOT Having new images inside ?

1,325 Views
ayyappadasps
Contributor II

I am building the ota file for imx6 platform in Marshmallow. i obtained the ota zip file but it doesn't have new images, I am getting update in META data file only. I am not getting updated Boot.img and system.img

I had followed the below steps to get OTA File 

make otapackage

make PRODUCT=sabresd_6dq-eng otapackage -j4

Then zip file is created with compiled date by using ls -l command

->sabresd_6dq-ota-20160331-imx6q.zip

After unzip, ls -l command result as follows,

-rw-rw-r-- 1 zumi-02 zumi-02 8865064 Jul 14 2011 boot.img
-rw-rw-r-- 1 zumi-02 zumi-02 445440 Jul 14 2011 bootloader.img
-rw-rw-r-- 1 zumi-02 zumi-02 15407 Jul 14 2011 file_contexts
-rw-r--r-- 1 zumi-02 zumi-02 271684670 May 22 20:21 sabresd_6dq-ota-20160331-imx6q.zip
-rw-rw-r-- 1 zumi-02 zumi-02 536703003 Jul 14 2011 system.new.dat
-rw-rw-r-- 1 zumi-02 zumi-02 0 Jul 14 2011 system.patch.dat
-rw-rw-r-- 1 zumi-02 zumi-02 345 Jul 14 2011 system.transfer.list

Can anyone help me to resolve this issue to get updated Images.

Labels (2)
Tags (2)
0 Kudos
9 Replies

843 Views
ayyappadasps
Contributor II

The reboot recovery log

0 Kudos

843 Views
ayyappadasps
Contributor II

hi Rita,

  After giving the command

   reboot recovery

sabersd board not getting booted properly.

i am attaching  log files of following

1. normal boot

2.procedure

3.reboot recovery log

waiting for your replay.

0 Kudos

843 Views
ayyappadasps
Contributor II

Hi Rita,

           Bsp i am using is android 6.0.1.

0 Kudos

843 Views
ayyappadasps
Contributor II

Hi Rita,

       Thanks first of all

    i done the following command      

make dist

but no update in zip file

0 Kudos

843 Views
ayyappadasps
Contributor II

ritayang      i am attaching the test case for "signature failed" in reboot recovery .

                 i am attaching the log of the failure in the below file.

0 Kudos

843 Views
ayyappadasps
Contributor II

Supported API: 3
Finding update package...
I:Update location: /cache/sabresd_6dq-ota-20160331.zip
Opening update package...
I:read key e=3 hash=20
I:1 key(s) loaded from /res/keys
Verifying update package...
I:comment is 1746 bytes; signature 1728 bytes from end
I:failed to verify against RSA key 0
E:failed to verify whole-file signature
I:verify_file returned 1
E:signature verification failed
Installation aborted.
I:timed out waiting for key input; rebooting.

0 Kudos

843 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

Please read the attachment file, it will help you.
Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

843 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

You can refer to the follow threads, hope these can do help for you.

Verification OTA w/ update.zip and diff-ota.zip 

iMX6q sabersd OTA update
Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

843 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

Which version BSP are you using?

Have a nice day

Rita

0 Kudos