requires libc.so.6(GLIBC_2.4), but no providers found in RDEPENDS_MediaLib-dev? [file-rdeps]

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

requires libc.so.6(GLIBC_2.4), but no providers found in RDEPENDS_MediaLib-dev? [file-rdeps]

11,655件の閲覧回数
ponguru_s
Contributor III

ERROR: MediaLib-0.1-r0 do_package_qa: QA Issue: -dev package contains non-symlink .so: MediaLib-dev path 'work/cortexa9hf-neon-poky-linux-gnueabi/MediaLib/0.1-r0/packages-split/MediaLib-dev/usr/lib/libMediaLibrary.so' [dev-elf]
WARNING: MediaLib-0.1-r0 do_package_qa: QA Issue: /usr/lib/libMediaLibrary.so contained in package MediaLib-dev requires libc.so.6(GLIBC_2.4), but no providers found in RDEPENDS_MediaLib-dev? [file-rdeps]
ERROR: MediaLib-0.1-r0 do_package_qa: QA run found fatal errors. Please consider fixing them.
ERROR: MediaLib-0.1-r0 do_package_qa: Function failed: do_package_qa
ERROR: Logfile of failure stored in: /home/user1/AGL_BUILD/fsl-arm-yocto-bsp/<my_build_dir>/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/MediaLib/0.1-r0/temp/log.do_package_qa.24842
ERROR: Task 9 (/home/user1/AGL_BUILD/fsl-arm-yocto-bsp/sources/meta-sample/recipes-mw/medialib/MediaLib_0.1.bb, do_package_qa) failed with exit code '1'
NOTE: Tasks Summary: Attempted 364 tasks of which 363 didn't need to be rerun and 1 failed.

MediaLib is the dynamic shared object created based upon my own requirements.

This has been the error I'm facing and unable to get any references to resolve this issue. Please help me with this.

ラベル(2)
0 件の賞賛
返信
5 返答(返信)

4,597件の閲覧回数
el14
Contributor II

Renaming the bb file without caps ,underscore etc have solved the same issue for me!

3,999件の閲覧回数
Jackie_Zhou
Contributor II
Geting rid of all caps helps slove the problems, Thanks!
0 件の賞賛
返信

7,132件の閲覧回数
tedwu
Contributor I

I also have the same problem.  It shows as follows.

WARNING: recordingAgent-3-r0 do_package_qa: QA Issue: /usr/bin/recordingAgent contained in package recordingAgent requires libc.so.6(GLIBC_2.4), but no providers found in RDEPENDS_recordingAgent? [file-rdeps]

But the library of libc.so.6 is at the folder of tmp/sysroots/imx7dsabresd/lib.

Can anyone tell me how to solve it?

0 件の賞賛
返信

7,132件の閲覧回数
ponguru_s
Contributor III

SUMMARY = "Media Library"
SECTION = "examples"
LICENSE = "MIT"

BB_STRICT_CHECKSUM = "0"
LIC_FILES_CHKSUM = "file://${COMMON_LICENSE_DIR}/MIT;md5=0835ade698e0bcf8506ecda2f7b4f302"

SRC_URI = "your_source_files"

S = "${WORKDIR}"
VER = "1"
HASHSTYLE = "gnu"

do_compile () {
${CC} -fPIC -shared -Wl,--hash-style=${HASHSTYLE} -o libMediaLibrary.so.${VER} -Wl,-soname,libMediaLibrary.so.${VER} source_files 
}

do_install() {
install -Dm755 ${B}/libMediaLibrary.so.${VER} ${D}${libdir}/libMediaLibrary.so.${VER}
ln -sf libMediaLibrary.so.${VER} ${D}${libdir}/libMediaLibrary.so
}

You can compare your code with the code mentioned above in the respective recipe file and try running the bitbake. The bold-italic terms are to be modified according to your library and source files.

The error is because no soft link is available.

Please let me know the status. :smileyhappy:

7,132件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

maybe you can downlaod the source package,

<RPM resource libc.so.6 >.

0 件の賞賛
返信