Hello NXP,
Using IMX6 to connect WIFI by PCIE, I want to save more power, so I removed the WIFI driver during sleep. After waking up, the PCIE is abnormal, and the WIFI driver cannot be installed. Please help analyze this problem?
Please check the following logs:
1. pcieport 0000:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring
2. 01:00.0 Network controller: Broadcom Limited Device 4415 (rev ff) (prog-if ff)
!!! Unknown header type 7f
Kernel modules: bcmdhd
3. The hardware resets the WIFI module. After scanning, you can see the WIFI, but the driver still cannot be installed.
log:
root@ctx0800-c0:~# lsmod
Module Size Used by
ip6table_mangle 16384 0
ip6_tables 28672 1 ip6table_mangle
iptable_mangle 16384 0
crc32_ce 16384 2
crct10dif_ce 16384 0
galcore 434176 0
root@ctx0800-c0:~# echo "1" > /sys/bus/pci/rescan
[ 4654.526737] bus_rescan_store 1 grayli
[ 4654.530511] pcieport 0000:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring
root@ctx0800-c0:~# echo "1" > /sys/bus/pci/rescan
[ 4702.474723] bus_rescan_store 1 grayli
root@ctx0800-c0:~# echo "1" > /sys/bus/pci/rescan
[ 4704.966706] bus_rescan_store 1 grayli
root@ctx0800-c0:~# lspci -v
00:00.0 PCI bridge: Freescale Semiconductor Inc Device 0000 (rev 01) (prog-if 00 [Normal decode])
Flags: fast devsel, IRQ 410
Memory at 70000000 (64-bit, non-prefetchable) [disabled] [size=16M]
Bus: primary=00, secondary=01, subordinate=01, sec-latency=0
I/O behind bridge: 00000000-00000fff [size=4K]
Memory behind bridge: 00000000-000fffff [size=1M]
Prefetchable memory behind bridge: 0000000000000000-00000000000fffff [size=1M]
[virtual] Expansion ROM at 71000000 [disabled] [size=16M]
Capabilities: [40] Power Management version 3
Capabilities: [50] MSI: Enable- Count=1/16 Maskable- 64bit+
Capabilities: [70] Express Root Port (Slot-), MSI 00
Capabilities: [100] Advanced Error Reporting
Capabilities: [148] #19
Capabilities: [168] L1 PM Substates
Kernel driver in use: pcieport
01:00.0 Network controller: Broadcom Limited Device 4415 (rev ff) (prog-if ff)
!!! Unknown header type 7f
Kernel modules: bcmdhd
ib/firmware/nf3323pq/4359_cypress_auto.clm_blobe/nf3323pq/bcmdhd.cal clm_path=/li
[ 4725.221569] pcieh 0000:01:00.0: of_irq_parse_pci-->pci_read_config_byte: rc=134 pin=255
[ 4725.229673] pcieh 0000:01:00.0: of_irq_parse_pci: failed with rc=134
[ 4725.236110] PCI_PROBE: bus 1, slot 0,vendor 14E4, device 4415(good PCI location)
[ 4725.262345] pcieh 0000:01:00.0: Refused to change power state, currently in D3
[ 4725.269999] Error creating socket.
insmod: ERROR: could not insert module /lib/modules/bcmdhd.ko: Operation not permitted
root@ctx0800-c0:~# [ 4739.384347] fec 5b040000.ethernet eth0: Link is Up - 1Gbps/Full - flow control off
root@ctx0800-c0:~# echo "1" > /sys/bus/pci/rescan
[ 4770.582716] bus_rescan_store 1 grayli
root@ctx0800-c0:~# [ 4812.088354] fec 5b040000.ethernet eth0: Link is Up - 1Gbps/Full - flow control off
root@ctx0800-c0:~# echo "1" > /sys/bus/pci/rescan
[ 4818.670697] bus_rescan_store 1 grayli
[ 4818.674444] pcieport 0000:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring
root@ctx0800-c0:~# echo "1" > /sys/bus/pci/rescan
[ 4821.310713] bus_rescan_store 1 grayli
root@ctx0800-c0:~# lspci -v
00:00.0 PCI bridge: Freescale Semiconductor Inc Device 0000 (rev 01) (prog-if 00 [Normal decode])
Flags: fast devsel, IRQ 410
Memory at 70000000 (64-bit, non-prefetchable) [disabled] [size=16M]
Bus: primary=00, secondary=01, subordinate=01, sec-latency=0
I/O behind bridge: 00000000-00000fff [size=4K]
Memory behind bridge: 00000000-000fffff [size=1M]
Prefetchable memory behind bridge: 0000000000000000-00000000000fffff [size=1M]
[virtual] Expansion ROM at 71000000 [disabled] [size=16M]
Capabilities: [40] Power Management version 3
Capabilities: [50] MSI: Enable- Count=1/16 Maskable- 64bit+
Capabilities: [70] Express Root Port (Slot-), MSI 00
Capabilities: [100] Advanced Error Reporting
Capabilities: [148] #19
Capabilities: [168] L1 PM Substates
Kernel driver in use: pcieport
01:00.0 Network controller: Broadcom Limited Device 4415 (rev 0d)
Subsystem: Broadcom Limited Device 0751
Flags: fast devsel
Memory at 72400000 (64-bit, non-prefetchable) [disabled] [size=32K]
Memory at 72000000 (64-bit, non-prefetchable) [disabled] [size=4M]
Capabilities: [48] Power Management version 3
Capabilities: [58] MSI: Enable- Count=1/16 Maskable- 64bit+
Capabilities: [68] Vendor Specific Information: Len=44 <?>
Capabilities: [ac] Express Endpoint, MSI 00
Capabilities: [100] Advanced Error Reporting
Capabilities: [13c] Device Serial Number 00-00-38-ff-ff-00-38-0f
Capabilities: [150] Power Budgeting <?>
Capabilities: [160] Virtual Channel
Capabilities: [1b0] Latency Tolerance Reporting
Capabilities: [220] #15
Capabilities: [240] L1 PM Substates
ib/firmware/nf3323pq/4359_cypress_auto.clm_blobe/nf3323pq/bcmdhd.cal clm_path=/l
[ 4838.797340] pcieh 0000:01:00.0: of_irq_parse_pci-->pci_read_config_byte: rc=0 pin=1
[ 4838.805122] pcieport 0000:00:00.0: of_irq_parse_pci-->of_irq_parse_raw: rc=0
[ 4838.812250] PCI_PROBE: bus 1, slot 0,vendor 14E4, device 4415(good PCI location)
[ 4838.819804] pcieh 0000:01:00.0: enabling device (0000 -> 0002)
[ 4838.826425] Error creating socket.
insmod: ERROR: could not insert module /lib/modules/bcmdhd.ko: Operation not permitted
root@ctx0800-c0:~#
root@ctx0800-c0:~# uname -a
Linux ctx0800-c0 4.14.98+g6c3e05d #1 SMP PREEMPT Fri Jan 21 13:49:43 UTC 2022 aarch64 aarch64 aarch64 GNU/Linux