Hi,everyone
Recently debuging ov5640_mipi ,Format is V4L2_PIX_FMT_UYVY ,Resolution is6440*480,I use mxc_v4l2_capture ,
but the image of getting has wrong Resolution , Can anyone Help me?
I change my ov5640 to ipu0 csi0 and the image captured is right,but I do not know why ipu1 csi0 doesn't work right.
one can check the bit 19 MIPI_IPU1_MUX of IOMUXC_GPR1 register.
pls refer to the enclose file to check if you set the mipi correct or not.
hi xie,
now i has get the right image when i Restore to the most original code, I modified the code not to work for reasons not yet found,I use ipu1 csi0.