no sound with SAI IMX7D as master, codec tlv320aic3104

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

no sound with SAI IMX7D as master, codec tlv320aic3104

跳至解决方案
1,962 次查看
mathad22
Contributor III

Hi there,

I am trying to switch my codec configuration to set the SAI of my IMX7D as master as I want to multiplex several codecs with the same SAI, my codec is TI tlv320aic3104.

My Linux kernel version is iMX 4.14.

I've changed my configuration but can't hear sound when I run some tests with speaker-test.

Here is my config, any idea of what is wrong?

 

 

 

&sai2 {
	#sound-dai-cells = <1>;
	pinctrl-names = "default";
	pinctrl-0 = <&pinctrl_sai2 &pinctrl_codec_reset &pinctrl_audio_ctrl>;
	assigned-clocks = <&clks IMX7D_SAI2_ROOT_SRC>,
			  <&clks IMX7D_SAI2_ROOT_CLK>;
	assigned-clock-parents = <&clks IMX7D_PLL_AUDIO_POST_DIV>;
	assigned-clock-rates = <0>, <12288000>;
	fsl,sai-synchronous-rx;
	fsl,sai-mclk-direction-output;
	status = "okay";
};

 

 

 

 

 

	sound-codec {
		compatible = "simple-audio-card";
		status = "okay";
		simple-audio-card,name = "EG4-Sound-Card";
		simple-audio-card,format = "i2s";
		simple-audio-card,bitclock-master = <&dailink0_master>;
		simple-audio-card,frame-master = <&dailink0_master>;

		simple-audio-card,widgets =
			"Speaker", "Speaker",
			"Line", "LineOut",
			"Headphone", "Ambient",
			"Microphone", "SpeakerMic",
			"Microphone", "AmbientMic";
		simple-audio-card,routing =
			"Speaker", "LLOUT",
			"LineOut", "RLOUT",
			"Ambient", "HPLOUT",
			"LINE1L", "SpeakerMic",
			"LINE1R", "AmbientMic";

		dailink0_master: simple-audio-card,cpu {
			sound-dai = <&sai2 0>;
			system-clock-frequency = <12288000>;
		};

		simple-audio-card,codec {
			sound-dai = <&tlv320aic3104>;
			clocks = <&clks IMX7D_SAI2_ROOT_CLK>;
			system-clock-frequency = <12288000>;
		};
	};

 

 

 

 

 

		tlv320aic3104: tlv320aic3104@18 {
			#sound-dai-cells = <0>;
			compatible = "ti,tlv320aic3104";
			reg = <0x18>;
			gpio-reset = <&gpio2 10 0>;
			clocks = <&clks IMX7D_SAI2_ROOT_CLK>;
			clock-names = "mclk";
			assigned-clocks = <&clks IMX7D_PLL_AUDIO_POST_DIV>,
					  <&clks IMX7D_AUDIO_MCLK_ROOT_DIV>;
			assigned-clock-rates = <884736000>,
			       		       <12288000>;

			AVDD-supply = <&avdd>;
			DRVDD-supply = <&avdd>;
			IOVDD-supply = <&iovdd>;
			DVDD-supply = <&dvdd>;
		};

 

 

 

 

 

		pinctrl_sai2: sai2grp {
			fsl,pins = <
				MX7D_PAD_SAI1_MCLK__SAI2_MCLK	0x04
				MX7D_PAD_SAI2_TX_BCLK__SAI2_TX_BCLK	0x1c
				MX7D_PAD_SAI2_TX_SYNC__SAI2_TX_SYNC	0x1c
				MX7D_PAD_SAI2_TX_DATA__SAI2_TX_DATA0	0x04
				MX7D_PAD_SAI2_RX_DATA__SAI2_RX_DATA0	0x1c
			>;
		};

 

 

 

 

 

Many thanks,

 

标签 (1)
0 项奖励
回复
1 解答
1,608 次查看
mathad22
Contributor III

I finally found the answer to my question, it seems that there is an issue on iMX7D SoC as mentioned on this document  https://www.nxp.com/docs/en/errata/IMX7DS_3N09P.pdf page 14.

ERR011096: SAI: Internal bit clock is not generated when RCR2[BCI]=1 or TCR2[BCI]=1
Description
When the SAI transmitter or receiver is configured for internal bit clock with BCI = 1, the bit clock is not generated for either of the
following two configurations:
a) SYNC = 00 and BCS = 0
b) SYNC = 01 and BCS = 1
Workaround
When the SAI transmitter or receiver is configured for internal bit clock with BCI=1, use only one of the following two configurations:
a) SYNC = 01 and BCS = 0
b) SYNC = 00 and BCS = 1

The solution to set the SAI as master is to create a kind of mix between a master/slave configuration, this probably requires a workaround from an HW point of view.

It seems also that the classic GPIOs have to be redirected because of that issue, here is an example between my configuration and another one from Variscite of what it could look like :

I voluntarily switched to SAI1

 

&sai1 {
	#sound-dai-cells = <1>;
	pinctrl-names = "default";
	pinctrl-0 = <&pinctrl_sai1 &pinctrl_sai1_mclk>;
	assigned-clocks = <&clks IMX7D_SAI1_ROOT_SRC>,
			  <&clks IMX7D_SAI1_ROOT_CLK>;
	assigned-clock-parents = <&clks IMX7D_PLL_AUDIO_POST_DIV>;
	assigned-clock-rates = <0>, <36864000>;
	status = "okay";
};

&clks {
	assigned-clocks = <&clks IMX7D_PLL_AUDIO_POST_DIV>;
	assigned-clock-rates = <884736000>;
};
	sound-codec {
		compatible = "simple-audio-card";
		status = "okay";
		simple-audio-card,name = "EG4-Sound-Card";
		simple-audio-card,widgets =
			"Speaker", "Speaker",
			"Line", "LineOut",
			"Headphone", "Ambient",
			"Microphone", "SpeakerMic",
			"Microphone", "AmbientMic";
		simple-audio-card,routing =
			"Speaker", "LLOUT",
			"LineOut", "RLOUT",
			"Ambient", "HPLOUT",
			"LINE1L", "SpeakerMic",
			"LINE1R", "AmbientMic";
		simple-audio-card,format = "i2s";
		simple-audio-card,bitclock-master = <&dailink0_master>;
		simple-audio-card,frame-master = <&dailink0_master>;

		/*simple-audio-card,bitclock-inversion;*/
		assigned-clocks = <&clks IMX7D_AUDIO_MCLK_ROOT_SRC>,
				  <&clks IMX7D_AUDIO_MCLK_ROOT_CLK>;
		assigned-clock-parents = <&clks IMX7D_PLL_AUDIO_POST_DIV>;
		assigned-clock-rates = <0>, <12288000>;

		dailink0_master: simple-audio-card,cpu {
			sound-dai = <&sai1 0>;
		};

		simple-audio-card,codec {
			sound-dai = <&tlv320aic3104>;
			system-clock-frequency = <12288000>;
		};
	};
		tlv320aic3104: tlv320aic3104@18 {
			#sound-dai-cells = <0>;
			compatible = "ti,tlv320aic3104";
			reg = <0x18>;
			gpio-reset = <&gpio2 10 0>;
			clocks = <&clks IMX7D_AUDIO_MCLK_ROOT_CLK>;
			clock-names = "mclk";

			AVDD-supply = <&avdd>;
			DRVDD-supply = <&avdd>;
			IOVDD-supply = <&dvdd>;
			DVDD-supply = <&dvdd>;
		};

 

GPIOs configuration to be tested and confirmed but the classic SAI outputs can't be used in that case and must be redirected to LPSR GPIOs:

 

		pinctrl_sai1: sai1grp {
			fsl,pins = <
				MX7D_PAD_ENET1_RX_CLK__SAI1_TX_BCLK	0x1f
				MX7D_PAD_ENET1_CRS__SAI1_TX_SYNC	0x1f
				MX7D_PAD_ENET1_COL__SAI1_TX_DATA0	0x30
				MX7D_PAD_ENET1_TX_CLK__SAI1_RX_DATA0	0x1f
			>;
		};

		pinctrl_sai1_mclk: sai1grp_mclk {
			fsl,pins = <
				MX7D_PAD_LPSR_GPIO1_IO01__SAI1_MCLK		0x1f
			>;
		};

 

在原帖中查看解决方案

0 项奖励
回复
10 回复数
1,609 次查看
mathad22
Contributor III

I finally found the answer to my question, it seems that there is an issue on iMX7D SoC as mentioned on this document  https://www.nxp.com/docs/en/errata/IMX7DS_3N09P.pdf page 14.

ERR011096: SAI: Internal bit clock is not generated when RCR2[BCI]=1 or TCR2[BCI]=1
Description
When the SAI transmitter or receiver is configured for internal bit clock with BCI = 1, the bit clock is not generated for either of the
following two configurations:
a) SYNC = 00 and BCS = 0
b) SYNC = 01 and BCS = 1
Workaround
When the SAI transmitter or receiver is configured for internal bit clock with BCI=1, use only one of the following two configurations:
a) SYNC = 01 and BCS = 0
b) SYNC = 00 and BCS = 1

The solution to set the SAI as master is to create a kind of mix between a master/slave configuration, this probably requires a workaround from an HW point of view.

It seems also that the classic GPIOs have to be redirected because of that issue, here is an example between my configuration and another one from Variscite of what it could look like :

I voluntarily switched to SAI1

 

&sai1 {
	#sound-dai-cells = <1>;
	pinctrl-names = "default";
	pinctrl-0 = <&pinctrl_sai1 &pinctrl_sai1_mclk>;
	assigned-clocks = <&clks IMX7D_SAI1_ROOT_SRC>,
			  <&clks IMX7D_SAI1_ROOT_CLK>;
	assigned-clock-parents = <&clks IMX7D_PLL_AUDIO_POST_DIV>;
	assigned-clock-rates = <0>, <36864000>;
	status = "okay";
};

&clks {
	assigned-clocks = <&clks IMX7D_PLL_AUDIO_POST_DIV>;
	assigned-clock-rates = <884736000>;
};
	sound-codec {
		compatible = "simple-audio-card";
		status = "okay";
		simple-audio-card,name = "EG4-Sound-Card";
		simple-audio-card,widgets =
			"Speaker", "Speaker",
			"Line", "LineOut",
			"Headphone", "Ambient",
			"Microphone", "SpeakerMic",
			"Microphone", "AmbientMic";
		simple-audio-card,routing =
			"Speaker", "LLOUT",
			"LineOut", "RLOUT",
			"Ambient", "HPLOUT",
			"LINE1L", "SpeakerMic",
			"LINE1R", "AmbientMic";
		simple-audio-card,format = "i2s";
		simple-audio-card,bitclock-master = <&dailink0_master>;
		simple-audio-card,frame-master = <&dailink0_master>;

		/*simple-audio-card,bitclock-inversion;*/
		assigned-clocks = <&clks IMX7D_AUDIO_MCLK_ROOT_SRC>,
				  <&clks IMX7D_AUDIO_MCLK_ROOT_CLK>;
		assigned-clock-parents = <&clks IMX7D_PLL_AUDIO_POST_DIV>;
		assigned-clock-rates = <0>, <12288000>;

		dailink0_master: simple-audio-card,cpu {
			sound-dai = <&sai1 0>;
		};

		simple-audio-card,codec {
			sound-dai = <&tlv320aic3104>;
			system-clock-frequency = <12288000>;
		};
	};
		tlv320aic3104: tlv320aic3104@18 {
			#sound-dai-cells = <0>;
			compatible = "ti,tlv320aic3104";
			reg = <0x18>;
			gpio-reset = <&gpio2 10 0>;
			clocks = <&clks IMX7D_AUDIO_MCLK_ROOT_CLK>;
			clock-names = "mclk";

			AVDD-supply = <&avdd>;
			DRVDD-supply = <&avdd>;
			IOVDD-supply = <&dvdd>;
			DVDD-supply = <&dvdd>;
		};

 

GPIOs configuration to be tested and confirmed but the classic SAI outputs can't be used in that case and must be redirected to LPSR GPIOs:

 

		pinctrl_sai1: sai1grp {
			fsl,pins = <
				MX7D_PAD_ENET1_RX_CLK__SAI1_TX_BCLK	0x1f
				MX7D_PAD_ENET1_CRS__SAI1_TX_SYNC	0x1f
				MX7D_PAD_ENET1_COL__SAI1_TX_DATA0	0x30
				MX7D_PAD_ENET1_TX_CLK__SAI1_RX_DATA0	0x1f
			>;
		};

		pinctrl_sai1_mclk: sai1grp_mclk {
			fsl,pins = <
				MX7D_PAD_LPSR_GPIO1_IO01__SAI1_MCLK		0x1f
			>;
		};

 

0 项奖励
回复
1,896 次查看
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

Are you able to hear something using an audio file.

If speaker test works, the sound card should be able to reproduce audio.

Best regards.

0 项奖励
回复
1,877 次查看
mathad22
Contributor III

Hi Jorge,

When the codec is master, yes, I can. But if it's the SAI as master, then I can't hear any sound.

 

0 项奖励
回复
1,864 次查看
JorgeCas
NXP TechSupport
NXP TechSupport

Got it.

Is the MPU providing the clock signal?

Did you check signals from the MPU to the codec?

Best regards.

0 项奖励
回复
1,850 次查看
mathad22
Contributor III

Hi Jorge,

I don't have an oscilloscope, but this is the next step.

I don't see another option to debug that issue, I will let you know.

 

0 项奖励
回复
1,810 次查看
mathad22
Contributor III

Hi Jorge here are the clocks and something goes wrong:

WCLK:

wclk

BLCK:

bclk

MCLK:

mclk

DIN:

din

DOUT:

dout

0 项奖励
回复
1,786 次查看
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

Yes, you should have something like this:

Jorge7u7_0-1691619953435.png

I suggest you check the reference device tree for i.MX7D or the reference device tree for i.MX8MM that also uses "simple-audio-card".

Best regards.

0 项奖励
回复
1,926 次查看
JorgeCas
NXP TechSupport
NXP TechSupport

Hello, I hope you are doing well.

You said, "I've changed my configuration but can't hear sound when I run some tests with speaker-test", did you was able to hear sound from the codec with a previous configuration?

I suggest you take a look at Chapter 16 Porting Audio Codecs i.MX Porting Guide.

Best regards.

0 项奖励
回复
1,911 次查看
mathad22
Contributor III

Hi Jorge,

Yes, I did, with the same i2s and i2c configuration and the codec as master, I can hear sound, here are more logs :

 

[    3.782982] asoc-simple-card sound-codec: tlv320aic3x-hifi <-> 308b0000.sai mapping ok
[    3.796342] rtc-pcf85063 3-0051: setting system clock to 2023-08-01 07:41:03 UTC (1690875663)
[    3.820909] usb_otg1_vbus: disabling
[    3.824515] A3V3: disabling
[    3.827327] D3V3: disabling
[    3.830174] D1V8: disabling
[    3.832987] VDD_SD1: disabling
[    3.836070] ALSA device list:
[    3.839076]   #0: EG4-Sound-Card

 

 

 

root@hdl-eg4:~# aplay -L
null
    Discard all samples (playback) or generate zero samples (capture)
sysdefault:CARD=EG4SoundCard
    EG4-Sound-Card, 
    Default Audio Device

 

 

 

root@hdl-eg4:~# speaker-test -Dsysdefault:CARD=EG4SoundCard -f 4000 -tsine -S 100 

speaker-test 1.2.1

Playback device is sysdefault:CARD=EG4SoundCard
Stream parameters are 48000Hz, S16_LE, 1 channels
Sine wave rate is 4000.0000Hz
Rate set to 48000Hz (requested 48000Hz)
Buffer size range from 64 to 16384
Period size range from 32 to 8192
Using max buffer size 16384
Periods = 4
was set period_size = 4096
was set buffer_size = 16384
 0 - Front Left
Time per period = 2.653695
 0 - Front Left
Time per period = 2.986700
 0 - Front Left

 

 

As you can see speaker-test works well but I can't hear no sound.

0 项奖励
回复
1,905 次查看
mathad22
Contributor III

Same test but codec is master :

[   70.836270] fsl-sai 308b0000.sai: ASoC: Store rate : 48000
[   96.522594] fsl-sai 308b0000.sai: ASoC: Store rate : 48000
[  340.312911] fsl-sai 308b0000.sai: ASoC: Store rate : 48000
root@hdl-eg4:~# alsamixer -c1
root@hdl-eg4:~# speaker-test -Dsysdefault:CARD=EG4SoundCard -f 4000 -tsine -S 100 

speaker-test 1.2.1

Playback device is sysdefault:CARD=EG4SoundCard
Stream parameters are 48000Hz, S16_LE, 1 channels
Sine wave rate is 4000.0000Hz
Rate set to 48000Hz (requested 48000Hz)
Buffer size range from 64 to 16384
Period size range from 32 to 8192
Using max buffer size 16384
Periods = 4
was set period_size = 4096
was set buffer_size = 16384
 0 - Front Left
Time per period = 2.653926
 0 - Front Left
Time per period = 2.986455
 0 - Front Left
Time per period = 2.98
0 项奖励
回复