MX53-LOCO u-boot and kernel image . Not able to boot till ROOT prompt(Username).
Please help me debug this issue.
On console I'm continuosly getting:
starting pid 2215, tty '': '/sbin/getty -L ttymxc0 115200 vt100'
process '/sbin/getty -L ttymxc0 115200 vt100' (pid 2215) exited. Scheduling for restart.
log obtained uImage :
EXT3-fs: barriers not enabled
kjournald starting. Commit interval 5 seconds
EXT3-fs (mmcblk0p1): using internal journal
EXT3-fs (mmcblk0p1): mounted filesystem with writeback data mode
VFS: Mounted root (ext3 filesystem) on device 179:1.
Freeing init memory: 172K
starting pid 1203, tty '': '/etc/rc.d/rcS'
Mounting /proc and /sys
Starting the hotplug events dispatcher udevd
Synthesizing initial hotplug events
Setting the hostname to freescale
Mounting filesystems
cp: write error: No space left on device
cp: write error: No space left on device
cp: write error: No space left on device
cp: write error: No space left on device
mount: mounting usbfs on /proc/bus/usb failed: No such file or directory
starting pid 2215, tty '': '/sbin/getty -L ttymxc0 115200 vt100'
process '/sbin/getty -L ttymxc0 115200 vt100' (pid 2215) exited. Scheduling for restart.
starting pid 2216, tty '': '/sbin/getty -L ttymxc0 115200 vt100'
process '/sbin/getty -L ttymxc0 115200 vt100' (pid 2216) exited. Scheduling for restart.
starting pid 2217, tty '': '/sbin/getty -L ttymxc0 115200 vt100'
------------------------------------------------------------------------------------
BOOTARGS:
Hit any key to stop autoboot: 3 2 0
MX53-LOCO U-Boot > printenv
bootdelay=3
baudrate=115200
loadaddr=0x70800000
netdev=eth0
ethprime=FEC0
uboot=u-boot.bin
kernel=uImage
nfsroot=/opt/eldk/arm
bootargs_nfs=setenv bootargs ${bootargs} root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp
bootcmd_net=run bootargs_base bootargs_nfs; tftpboot ${loadaddr} ${kernel}; bootm
bootcmd=run bootcmd_mmc
ethact=FEC0
bootcmd_mmc=run bootargs_base bootargs_mmc;mmc dev 0;mmc read ${loadaddr} 0x800 0x1800;bootm
bootargs_mmc=setenv bootargs ${bootargs} root=/dev/mmcblk0p1 rw rootwait
ethaddr=00:04:9f:01:32:e0
bootargs_base=setenv bootargs console=ttymxc0,115200
stdin=serial
stdout=serial
stderr=serial
That error sometimes happens due to too small TMPFS_SIZE in /etc/rc.d/rc.conf . Try increasing default size from 512k to 8192k and see if it fixes the problem.
cp:write error no space left on device is solved.
changed TMPFS_SIZE = 8192k in etc/rc.d/rc.conf
--------------------------------------------------------
.But still facing Issue.
starting pid 2215, tty ':'/sbin/getty -L ttymxc0 115200 vt100
process '/sbin/getty -L ttymxc0 115200 vt100'(pid 2215)exited.Scheduling for restart.
Hi omprakash,
Were you able to solve the issue. please let me know. I am also stuck at the same point.
Thanks.
Hi,
I have the same issue?
Have you solved the problem?
Best regards,
Matteo.
which profile you used to build in LTIB? if possible, please tell me the details and the steps so I can try to reproduct the problem on my side.
Hello, omprakash!
Please recheck you inittab, rcS and other scripts which run after starting system.