mx53 can‘t boot wince7 from SD Card

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mx53 can‘t boot wince7 from SD Card

Jump to solution
1,450 Views
JackyHuang
Contributor III

Dear All:

Im a newer in wince7.

Now my company design a mx53 board base on the mx53smd reference board. 

We just reduce the ddr from 1G to 512M!

we can't boot the wince7 from SD Card, there is no print output to the UART.

however, we can boot android from SD Card succeed.

so, what can I do to make the wince7 boot from SD Card succeed?

Thanks advance!

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
1,204 Views
king_jin
NXP Employee
NXP Employee

You need to configure the correct parameters for DDR memory in bootloader(hardware should help). Next you should define the IMGRAM512 macro in BSP manually.

View solution in original post

0 Kudos
Reply
3 Replies
1,204 Views
liaoaleon
Contributor I

I had the same problem,Can anyone tell me have configure it?!

0 Kudos
Reply
1,204 Views
JackyHuang
Contributor III

Thanks for your help,  I'll try it

0 Kudos
Reply
1,205 Views
king_jin
NXP Employee
NXP Employee

You need to configure the correct parameters for DDR memory in bootloader(hardware should help). Next you should define the IMGRAM512 macro in BSP manually.

0 Kudos
Reply