Hello all,
I've got custom mx53 board based on mx53 loco with mc34708 power and last 2.6.35 kernel from freescale git.
My MC34708 PMIC_INT connected to CSI0_DAT10 and muxed as gpio 5_28.
How to get power button to work?
AFAIK TZIC workaround needs to be used only for da9053 boards.
Some code below:
#if defined(CONFIG_KEYBOARD_GPIO) || defined(CONFIG_KEYBOARD_GPIO_MODULE)
#define GPIO_BUTTON(gpio_num, ev_code, act_low, descr, wake) \
{ \
.gpio = gpio_num, \
.type = EV_KEY, \
.code = ev_code, \
.active_low = act_low, \
.desc = "btn " descr, \
.wakeup = wake, \
}
static struct gpio_keys_button loco_buttons[] = {
GPIO_BUTTON(MX53_nONKEY, KEY_POWER, 1, "power", 0),
};
static struct gpio_keys_platform_data loco_button_data = {
.buttons = loco_buttons,
.nbuttons = ARRAY_SIZE(loco_buttons),
};
static struct platform_device loco_button_device = {
.name = "gpio-keys",
.id = -1,
.num_resources = 0,
.dev = {
.platform_data = &loco_button_data,
}
};
static void __init loco_add_device_buttons(void)
{
platform_device_register(&loco_button_device);
}
#else
static void __init loco_add_device_buttons(void) {}
#endif
static void mxc_register_powerkey(pwrkey_callback pk_cb)
{
pmic_event_callback_t power_key_event;
power_key_event.param = (void *)1;
power_key_event.func = (void *)pk_cb;
pmic_event_subscribe(EVENT_PWRONI, power_key_event);
}
static int mxc_pwrkey_getstatus(int id)
{
int sense;
pmic_read_reg(REG_INT_SENSE1, &sense, 0xffffffff);
if (sense & (1 << 3))
return 0;
return 1;
}
static struct power_key_platform_data pwrkey_data = {
.key_value = KEY_F4,
.register_pwrkey = mxc_register_powerkey,
.get_key_status = mxc_pwrkey_getstatus,
};
//-------- init
mc34708_int = MX53_PAD_CSI0_DAT10__GPIO5_28;
mx53_loco_mc34708_irq = (4*32 + 28);
mxc_iomux_v3_setup_pad(mc34708_int);
gpio_request(mx53_loco_mc34708_irq, "pmic-int");
gpio_direction_input(mx53_loco_mc34708_irq);
mx53_loco_init_mc34708(mx53_loco_mc34708_irq);
dvfs_core_data.reg_id = "SW1A";
tve_data.dac_reg = "VDAC";
bus_freq_data.gp_reg_id = "SW1A";
bus_freq_data.lp_reg_id = "SW2";
mxc_register_device(&mxc_powerkey_device, &pwrkey_data);
mxc_register_device(&pm_device, &loco_pm_data);
loco_add_device_buttons();
I can wakeup board thru USB, but cannot use button.
I even can't check gpio thru terminal:
echo 156 > sys/class/gpio/export
-bash: echo: write error: Device or resource busy
What's wrong with my configuration?
hello,alexeym,
I did it based on mc34708+i.mx53, please add the following:
/*Maybe you have these 4 lines in your BSP*/
#define TZIC_WAKEUP0_OFFSET (0x0E00)
#define TZIC_WAKEUP1_OFFSET (0x0E04)
#define TZIC_WAKEUP2_OFFSET (0x0E08)
#define TZIC_WAKEUP3_OFFSET (0x0E0C)
/*Use GPIO1_8 to control wakeup and sleep*/
#define GPIO1_8_18_IRQ_BIT (0x1<<18)
....
/*Following code should be adjusted*/
static void pad_tzic_irq_wakeup(void)
{
void __iomem *tzic_base;
tzic_base = ioremap(MX53_TZIC_BASE_ADDR, SZ_4K);
if (NULL == tzic_base) {
pr_err("fail to map MX53_TZIC_BASE_ADDR\n");
return;
}
__raw_writel(0, tzic_base + TZIC_WAKEUP0_OFFSET);
__raw_writel(0, tzic_base + TZIC_WAKEUP2_OFFSET);
__raw_writel(0, tzic_base + TZIC_WAKEUP3_OFFSET);
__raw_writel(GPIO1_8_18_IRQ_BIT, tzic_base + TZIC_WAKEUP1_OFFSET);
iounmap(tzic_base);
pr_info("TZIC irq is wakeup-enabled\n");
}
static void pad_suspend_enter(void)
{
pad_tzic_irq_wakeup();
}
static void pad_suspend_exit(void)
{
/*add your suppend exit code*/
printk(KERN_INFO "GPIO1_8 irq is to wakeup system\n");
}
static struct mxc_pm_platform_data pad_pm_data = {
.suspend_enter = pad_suspend_enter,
.suspend_exit = pad_suspend_exit,
};
....
/*following is your above code */
.....
.....
<Note: accroding to reference manul ,the interrupt number of GPIO_1 signal0~signal15 is 50, we can calculate wakeup bit in TZIC, see page 4622, 32x1+18 = 50, so we can find wakeup bit : No.18 bit in WAKEUP1 register. >
See attachment, for you as a reference. But you should notice that you can't clear wakeup source of USB. In my code ,I cleaned it.
Weidong