mmc0: Timeout waiting for hardware interrupt.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mmc0: Timeout waiting for hardware interrupt.

2,766件の閲覧回数
rajathks
Contributor II

I'm using IMX6UL processor having kernal version 4.1 which runs Ubuntu (ubuntu-base-16.04.2-base-armhf.tar.gz downloaded from http://cdimage.ubuntu.com/ubuntu-core/ ) operating system. For few days i was able to boot it from SD card with no issues. Few days later i noticed that the processor is in hang state. Now, While booting from SD card, at certain point booting hangs and throws the following error

mmc0: Timeout waiting for hardware interrupt.
random: nonblocking pool is initialized

Can someone give input on this like why it has happened & how can this is prevented ?


With Regards,
Raj

ラベル(4)
タグ(2)
0 件の賞賛
返信
2 返答(返信)

2,030件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Rajath,

The i.MX6UL support eMMC 4.0 don´t know if you are using other, however this issues is due to you downloaded a package that affects the eMMC functionality.

0 件の賞賛
返信

2,030件の閲覧回数
rajathks
Contributor II

Hi ,

Thanks for the reply. Is there any way to find which package is causing the problem ?

0 件の賞賛
返信