mipi

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mipi

698件の閲覧回数
sumosumo
Contributor I

hi imx community

i have ov5640 mipi of econsystem and i found that the driver (ov5640_mipi of 3.10.17 kernel) doesnt contain any registers configuration for hdmi.

did anyone managed to use hdmi anyhow with the driver mentioned above?

thanks!

0 件の賞賛
返信
1 返信

590件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi sumo

for hdmi input one can use parallel input (csi), for input through mipi one will have

to use additional external converter and modify sources, as below :

Some Experience When Enable MIPI Camera

https://community.freescale.com/thread/314211

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信