mfgtool for i.MX RT vs UUU tool for i.MX 6&8

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mfgtool for i.MX RT vs UUU tool for i.MX 6&8

1,658 Views
kanimozhi_t
Contributor V

Hi, is the MFGTool referred in i.MX RT manuals same as the opensource UUU tool (https://github.com/NXPmicro/mfgtools) for i.MX 6  & 8 processors.

kanimozhi_t_0-1651057979506.jpeg

We know that MFGTool is predecessor of UUU and UUU has the support for i.MX RT 106x devices. But are these two exactly the same?

Labels (1)
Tags (2)
0 Kudos
Reply
3 Replies

1,649 Views
joanxie
NXP TechSupport
NXP TechSupport

they are different,

joanxie_0-1651064783947.png

for difference between uuu script and mfgtools, you also can refer to the chapter 6 Migration from mfgtool ucl2.xml of enclosed file

 

1,633 Views
kanimozhi_t
Contributor V

Thank you @joanxie 

 

Yet we want to confirm the following once.

  1. UUU tool is supposed to replace MFGTool, correct?
  2. Can we flash/program i.MX RT (particularly RT 1160) with UUU tool?
0 Kudos
Reply

1,623 Views
joanxie
NXP TechSupport
NXP TechSupport

yes, uuu tool replace the mfgtools in i.mx8, it seems that i.mxRT doesn't support uuu tool

joanxie_1-1651151808993.png