There is an useful tool (m4ctl) for start/stop/deploy m4 from Linux but can't work on i.MX8M Mini.
We know there is an application note (AN5317) about similar function for i.MX6SX/i.MX7 can refered but just several detail steps instead of tool like above.
Is there simple command line tool like m4ctl for i.MX8M Mini?
https://source.codeaurora.org/external/imxsupport/m4ctrl/tree/README.md
解決済! 解決策の投稿を見る。
Hi m.c.
additional files were sent via mail.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear Igor,
is it possible to obtain the patches and instructions for iMX8MM/iMX8MQ?
Are we supposed to sign any NDA?
Thanks
Regards
Pier
Hi,
I would also be interested in information about running m4ctrl on imx8mq.
same here
Also need m4ctrl working on imx8mm.
Is there a standard implementation for the m4ctrl package for the i.MX8m mini?
Could I also get a copy of these files?
Hi m.c.
additional files were sent via mail.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
We also need this patch.
Please let me know what do you need from us.
Thanks in advance. Cheers,
Emilio
use the rpmsg_lite_str_echo_rtos M4 project, and the Linux side uses imx_rpmsg_tty.ko. 1: Normal uboot starts M4, after linux starts, load the module insmod imx_rpmsg_tty.ko 2: rpmsg str echo is normal 3: Use m4ctl in linux to reset M4 4: Uninstall the module rmmod imx_rpmsg_tty.ko 5: Reload insmod imx_rpmsg_tty.ko 6: The rpmsg str echo is abnormal, and the M4 is in an infinite loop while (!rpmsg_lite_is_link_up(my_rpmsg)); question1: How can I keep the rpmsg tty working normally after resetting M4 core using m4ctl in Linux?
Alse need m4ctrl working on imx8mm
Can you send same code to me?
Hi Igor
I often see your comment that you are sending the information via e-mail instead of posting here. Is there a reason for not posting those. As this is an open forum it would be nice to have the information available for all of us. Perhaps some of the stuff you send privately is related to the security part of the SoC and probably not available for public. Is this the case with this one as well ?
Best regards
Sinan Akman
Hi Sinan
it may be suggested to create service request for such cases.
https://community.nxp.com/docs/DOC-329745
Best regards
igor
Hi Igor
Perhaps you misunderstood. I was just asking why you sometimes (and for this particular case as well) send the replies via e-mail instead of posting here so that everyone can have access to the information.
Regards
Sinan Akman
Hi Sinan
I fully understood your question.
Not all internal codes can be publicly shared.
Regarding this patch I asked owner of this application
what could be better option to proceed.
Best regards
igor
Hi Igor
Thanks for your time responding to this. I totally understand there are some information e.g related to security issues etc. that can't be shared publicly. In this particular thread it would be great If the author (Stefan) was able to share the files you send individually. As I can see there is at least 3 other people who were interested in this. I guess my point and suggestion is as an open forum, replies should be open to everyone as much as possible since otherwise it looses its meaning to be an open forum becomes more of a technical support portal. However here we all like to share our technical experiences and would like refer to previous threads when we come across with a new problem.
This is my 2 cents and thanks for your consideration.
Best regards
Sinan Akman
Hi Sinan
Regarding this patch I asked owner of this application
what could be better option to proceed. His answer below
------------------------------
-------------------------------
Best regards
igor
I am also interested.
I think we have enough requests in order to publish the i.mx8 mini support.
Daniel.
Hi Igor,
access to the patch to use m4ctrl on i.MX8MQ would be very useful for me also, it would be great if this support gets added to the next release!
Best regards, Klaus