m4ctl for i.MX8M Mini

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

m4ctl for i.MX8M Mini

ソリューションへジャンプ
9,382件の閲覧回数
m_c
Senior Contributor I

There is an useful tool (m4ctl) for start/stop/deploy m4 from Linux but can't work on i.MX8M Mini.

We know there is an application note (AN5317) about similar function for i.MX6SX/i.MX7 can refered but just several detail steps instead of tool like above.

Is there simple command line tool like m4ctl for i.MX8M Mini?

https://source.codeaurora.org/external/imxsupport/m4ctrl/tree/README.md

http://nxp.com/doc/an5317

ラベル(1)
1 解決策
9,043件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi m.c.

additional files were sent via mail.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
20 返答(返信)
8,934件の閲覧回数
pierluigi_p
Senior Contributor I

Dear Igor,

is it possible to obtain the patches and instructions for iMX8MM/iMX8MQ?

Are we supposed to sign any NDA?

Thanks

Regards

Pier

0 件の賞賛
返信
9,043件の閲覧回数
Farsan_Baloo
Contributor II

Hi,

I would also be interested in information about running m4ctrl on imx8mq. 

0 件の賞賛
返信
9,043件の閲覧回数
davidvescovi
Contributor V

same here

0 件の賞賛
返信
9,043件の閲覧回数
pavel_
Contributor II

Also need m4ctrl working on imx8mm.

0 件の賞賛
返信
9,043件の閲覧回数
tracke
Contributor I

Is there a standard implementation for the m4ctrl package for the i.MX8m mini?
Could I also get a copy of these files?

0 件の賞賛
返信
9,044件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi m.c.

additional files were sent via mail.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
8,258件の閲覧回数
emilsedemil
Contributor II

Hi,

We also need this patch.

Please let me know what do you need from us.

Thanks in advance. Cheers,

Emilio

0 件の賞賛
返信
8,764件の閲覧回数
darcyxu
Contributor II

use the rpmsg_lite_str_echo_rtos M4 project, and the Linux side uses imx_rpmsg_tty.ko. 1: Normal uboot starts M4, after linux starts, load the module insmod imx_rpmsg_tty.ko 2: rpmsg str echo is normal 3: Use m4ctl in linux to reset M4 4: Uninstall the module rmmod imx_rpmsg_tty.ko 5: Reload insmod imx_rpmsg_tty.ko 6: The rpmsg str echo is abnormal, and the M4 is in an infinite loop while (!rpmsg_lite_is_link_up(my_rpmsg)); question1: How can I keep the rpmsg tty working normally after resetting M4 core using m4ctl in Linux?

0 件の賞賛
返信
8,992件の閲覧回数
dragonzhangcl
Contributor I

Alse need m4ctrl working on imx8mm

Can you send same code to me?

0 件の賞賛
返信
9,042件の閲覧回数
sinanakman
Senior Contributor III

Hi Igor

I often see your comment that you are sending the information via e-mail instead of posting here. Is there a reason for not posting those. As this is an open forum it would be nice to have the information available for all of us. Perhaps some of the stuff you send privately is related to the security part of the SoC and probably not available for public. Is this the case with this one as well ?

Best regards

Sinan Akman

0 件の賞賛
返信
9,042件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Sinan 

it may be suggested to create service request for such cases.

https://community.nxp.com/docs/DOC-329745 

Best regards
igor

0 件の賞賛
返信
9,042件の閲覧回数
sinanakman
Senior Contributor III

Hi Igor

Perhaps you misunderstood. I was just asking why you sometimes (and for this particular case as well) send the replies via e-mail instead of posting here so that everyone can have access to the information.

Regards

Sinan Akman

0 件の賞賛
返信
9,042件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Sinan 

 

I  fully understood your question.

Not all internal codes can be publicly shared.

Regarding this patch I asked owner of this application

what could be better option to proceed.

Best regards
igor

9,042件の閲覧回数
sinanakman
Senior Contributor III

Hi Igor

Thanks for your time responding to this. I totally understand there are some information e.g related to security issues etc. that can't be shared publicly. In this particular thread it would be great If the author (Stefan) was able to share the files you send individually. As I can see there is at least 3 other people who were interested in this. I guess my point and suggestion is as an open forum, replies should be open to everyone as much as possible since otherwise it looses its meaning to be an open forum becomes more of a technical support portal. However here we all like to share our technical experiences and would like refer to previous threads when we come across with a new problem.

This is my 2 cents and thanks for your consideration.

Best regards

Sinan Akman

0 件の賞賛
返信
9,042件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Sinan 

 

Regarding this patch I asked owner of this application

what could be better option to proceed. His answer below

------------------------------

pastedImage_1.jpg

pastedImage_2.jpg

------------------------------- 

Best regards
igor

0 件の賞賛
返信
8,963件の閲覧回数
dwainer
Contributor I

I am also interested.

I think we have enough requests in order to publish the i.mx8 mini support.

Daniel.

0 件の賞賛
返信
4,604件の閲覧回数
dwainer
Contributor I
I switched to remoteproc for controlling Cortex-M4. It can load firmware as well as control the processor start/stop state. the task can be performed many times, switching from firmware to firmware without rebooting.
0 件の賞賛
返信
4,595件の閲覧回数
AlexJLennon
Contributor III
That's really helpful thanks @dwainer - will go and investigate!
0 件の賞賛
返信
9,004件の閲覧回数
kuehnhammer
Contributor I

Hi Igor,

access to the patch to use m4ctrl on i.MX8MQ would be very useful for me also, it would be great if this support gets added to the next release!

Best regards, Klaus

0 件の賞賛
返信
4,609件の閲覧回数
AlexJLennon
Contributor III

Hi Igor,

We have a customer using Zephyr on the Cortex M4 and we could do with access to these utilities too.

Could  you send me the files also please?

Thakns

タグ(1)
0 件の賞賛
返信