Dear Community,
i installed ltib (Release L2.6.31_09.12.01) for the i.MX35. In the graphical configuration there are several
options to set so that they can be used in the Board Image. It seems that ethtool cannot be disabled.
I tried to build the image but it stopped with the message,
Processing: ethtool
=====================
Build path taken because: no prebuilt rpm,
Testing network connectivity
No network download connection available
Can't get: ethtool-3.tar.gz at ./ltib line 790.
f_buildrpms() returned an error, exiting
traceback:
main:560
Started: Fri Nov 7 08:39:50 2014
Ended: Fri Nov 7 08:40:02 2014
Elapsed: 12 seconds
These packages failed to build:
ethtool
Build Failed
Exiting on error or interrupt
How can i install the ethtool-3.tar.gz. I cannot find that package. Internet connectivity is established,
but where can i find this package?
Can anyone help me please.
已解决! 转到解答。
Hi Alexander
attached ethtool-3.tar.gz, you can put it
in /opt/freescale/pkgs directory.
If necessary you can search web and put necessary files
manually to that directory.
Best regards
igor
Hi Igor,
thanks for your fast reply.
But it hangs at the same stage.
Processing: ethtool
=====================
Build path taken because: no prebuilt rpm,
Testing network connectivity
No network download connection available
WARN: skipping md5sum check for /opt/freescale/pkgs/ethtool-3.tar.gz, md5 file was not found
Can't get: ethtool-3-fifo.patch at ./ltib line 790.
f_buildrpms() returned an error, exiting
traceback:
main:560
Do you know what the ethtool-3-fifo.patch is?
Is there a download page where the packages are available?
Regards,
Alexander Achleitner