ltib install ethtool-3.tar.gz

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ltib install ethtool-3.tar.gz

Jump to solution
1,431 Views
alexanderachlei
Contributor II

Dear Community,

i installed ltib (Release L2.6.31_09.12.01) for the i.MX35. In the graphical configuration there are several

options to set so that they can be used in the Board Image. It seems that ethtool cannot be disabled.

I tried to build the image but it stopped with the message,

Processing: ethtool
=====================
Build path taken because: no prebuilt rpm,
Testing network connectivity
No network download connection available

Can't get: ethtool-3.tar.gz at ./ltib line 790.


f_buildrpms() returned an error, exiting
traceback:
main:560


Started: Fri Nov  7 08:39:50 2014
Ended:   Fri Nov  7 08:40:02 2014
Elapsed: 12 seconds

These packages failed to build:
ethtool

Build Failed

Exiting on error or interrupt

How can i install the ethtool-3.tar.gz. I cannot find that package. Internet connectivity is established,

but where can i find this package?

Can anyone help me please.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,081 Views
igorpadykov
NXP Employee
NXP Employee

Hi Alexander

attached ethtool-3.tar.gz, you can put it

in /opt/freescale/pkgs directory.

If necessary you can search web and put necessary files

manually to that directory.

Best regards

igor

View solution in original post

0 Kudos
Reply
3 Replies
1,082 Views
igorpadykov
NXP Employee
NXP Employee

Hi Alexander

attached ethtool-3.tar.gz, you can put it

in /opt/freescale/pkgs directory.

If necessary you can search web and put necessary files

manually to that directory.

Best regards

igor

0 Kudos
Reply
1,081 Views
alexanderachlei
Contributor II

Hi Igor,

thanks for your fast reply.

But it hangs at the same stage.

Processing: ethtool
=====================
Build path taken because: no prebuilt rpm,
Testing network connectivity
No network download connection available

WARN: skipping md5sum check for /opt/freescale/pkgs/ethtool-3.tar.gz, md5 file was not found
Can't get: ethtool-3-fifo.patch at ./ltib line 790.


f_buildrpms() returned an error, exiting
traceback:
main:560

Do you know what the ethtool-3-fifo.patch is?

Is there a download page where the packages are available?

Regards,

Alexander Achleitner

0 Kudos
Reply
1,081 Views
alexanderachlei
Contributor II

Hi Igor,

ist me again. I downloaded the patch and this Problem is fixed.

Thank you very much.

Regards,

Alexander Achleitner