Hello support team,
Configuration
Build Configuration:
BB_VERSION = "2.0.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "universal"
TARGET_SYS = "arm-poky-linux-gnueabi"
MACHINE = "imx6qdlsabresd"
DISTRO = "fsl-imx-wayland"
DISTRO_VERSION = "5.15-kirkstone"
TUNE_FEATURES = "arm vfp cortexa9 neon thumb callconvention-hard"
TARGET_FPU = "hard"
meta
meta-poky = "HEAD:27de52e402ae000dfa502d52908cd6e6aef923ec"
meta-oe
meta-multimedia
meta-python = "HEAD:5357c7a40eaf8d1bcf7ff58edbba8e9527e40c7d"
meta-freescale = "HEAD:2fb1ce365338126aad365012ebb913b3e4a9f1be"
meta-freescale-3rdparty = "HEAD:de0eb1408150d77f9cce97c559f9a5a3c71e5d6c"
meta-freescale-distro = "HEAD:fc15f5003043da23212596be7366ae2547c308ad"
meta-bsp
meta-sdk
meta-ml
meta-v2x = "HEAD:5bc708f56575a878da17f2148e959c95d06cf8db"
meta-nxp-demo-experience = "HEAD:8fade3993b832ecd823771644f2a7b731f8f4527"
meta-chromium = "HEAD:d25d8ee98a656b2534d0eec6138ef264529fab4f"
meta-clang = "HEAD:85d956d95401479ca666139e31f662f60c156d5f"
meta-gnome
meta-networking
meta-filesystems = "HEAD:5357c7a40eaf8d1bcf7ff58edbba8e9527e40c7d"
meta-qt6 = "HEAD:b2894aad5c1aaa85f2f5c7b94391b7c51c39e555"
meta-virtualization = "HEAD:973c8d0964c6f40338857efe5b8009b2f647d485"
bitbake core-image-minimal
after building the image, flash the image into sd card by giving below command
bzcat <image_name>.wic.bz2 | sudo dd of=/dev/sd<partition> bs=1M conv=fsync
sudo fdisk /dev/sda -l Disk /dev/sda: 29.3 GiB, 31457280000 bytes, 61440000 sectors Units: sectors of 1 * 512 = 512 bytes Sector size (logical/physical): 512 bytes / 512 bytes I/O size (minimum/optimal): 512 bytes / 512 bytes Disklabel type: dos Disk identifier: 0x3f9d3c50 Device Boot Start End Sectors Size Id Type /dev/sda1 * 8192 60825 52634 25.7M c W95 FAT32 (LBA) /dev/sda2 65536 288921 223386 109.1M 83 Linux
question
usually three partition will be generated ? but from the above two partition are shown, is the above is correct
uboot.sb will be burned in partition1 (memory loader FSBL)
uimage and .dtb burned in partition2 (Uboot, environment variable)
rootfs,linux image(dev,etc......) burned in partition3 (rootfs, uimage)
please confirm
解決済! 解決策の投稿を見る。
Hi @shankovai
Two partitions are correct. U-boot, dtb, and kernel will be stored at first partition. Rootfs will be at second partition.
Best regards
Harvey
Hi @shankovai
Two partitions are correct. U-boot, dtb, and kernel will be stored at first partition. Rootfs will be at second partition.
Best regards
Harvey