Hello all,
I have I.MX28 custom board and run with default kernel(linux-2.6.35.3) and fs without any problem.
I have to upgrade kernel to linux-3.1 or higher. I tried linux-3.4.1.
I don't use uboot, use imx28_ivt_linux.sb image with sdcard.
I give path of new kernel for "kernel(Local Linux directory build)" config after "./ltib -m config". There is no problem, it was built and tried to run with new imx28_ivt_linux.sb but it hanged up after "Uncompressing Linux... done, booting the kernel" message.
I need your help, ideas..
Thanks
Mehmet
解決済! 解決策の投稿を見る。
If you want to do a kernel upgrade for mx28, then I would suggest the latest stable version, which is 3.8.4.
The console in the mainline kernel is ttyAMA0, instead of ttyAM0 in 2.6.35.
Using the mainline U-boot can make things easier as well, as it supports booting a device tree kernel.
It is also possible to boot via bootlets, but you need to create a combined zImage with dtb + zImage.
If you want to do a kernel upgrade for mx28, then I would suggest the latest stable version, which is 3.8.4.
The console in the mainline kernel is ttyAMA0, instead of ttyAM0 in 2.6.35.
Using the mainline U-boot can make things easier as well, as it supports booting a device tree kernel.
It is also possible to boot via bootlets, but you need to create a combined zImage with dtb + zImage.
Below is a link that to some relevant discussion. The likely change in the Kernel from 2.6.35.3 to 3.x is the inclusion of the dts/dtb files to setup the hardware. No hardware configuration, no UART configuration, no debug messages can be printed after "Linux is uncompressed" message. Below is a thread with some relevant information.