Hi,
We are using i.MX6 Solo processor. For that we are using boot mode 10 (internal boot mode) and done GPIO setting for boot from uSHC--2 (microSD card). But it is not booting from it. I have checked the clock and command lines, but I have not seen any activity there.
In boot mode 00, because of manufacturing mode it is booting from uSHC--2 (microSD card).
I have checked all the GPIO settings. For reference I have attaché d the GPIO settings.
With regards
LK
Yes. I have checked all gpio settings. Also checked cmd and clock lines with boot mode 00 and 10. In boot mode 10 there is no signal,while in boot mode 00 i was able to get the clock in oscilloscope.
CD is low then only it is booting from sd-2 in boot mode 00.
please check by oscilloscope voltages (_ARM_CAP,SOC_CAP,HIGH_CAP)
and clocks 24MHz,32.768KHz in both good and bad cases.
Check that ripple noise should be less than 5% Vp-p of supply voltage average value.
Also check if _CAP capacitors comply with latest recommendations below
HW Design Checking List for i.MX6DQSDL
~igor
VDDARM_CAP: 1.17V (pk-pk ripple 0.84%)
VDDSOC_CAP: 1.17V (pk-pk ripple 3.4%)
VDDHIGH_CAP: 2.52V (pk-pk ripple 1.78%)
24MHz and 32.768KHzboth are in good shape
We have taken care whatever mention in the checklist.
It is booting from SD-2 slot in boot mode 00. So I am just thinking, if there is any such issue, it should create problem there also. We are not able to get the clock or command signals itself. It means it is not even going to that step.
With regards
LK
- if this issue happens on one board or all (how many)
- could you provide full i.MX6 marking
- in bad case, does processor go to "Serial Downloader"
or just hangs ? If hangs, could you attach jtag and check where (address) ?
~igor
also please recheck that BOOT_CFG4[7]
(UART3_RTS ) not set to "1".
Table 8-2. Boot eFUSE Descriptions IMX6SDLRM
BOOT_CFG4[7]=1 Infinite Loop Enable at start
of boot ROM. Used for debugging purposes.