interaface of IMx6 Dual Core CPU and 10.1' inch TFT LCD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

interaface of IMx6 Dual Core CPU and 10.1' inch TFT LCD

839 Views
alpeshmandani
Contributor IV

We have use IMx6 Dual Core CPU and 10.1' inch TFT LCD in our Design. We need help for interfacing of LCD with IMX6 and we have following query.

  • our LCD support MIPI 4 Lane Interface and IMx6 Dual CPU support MIPI 2 Lane Interface , How we will Interface LCD with IMx6 processor?
  • Is there any possibly way to keep NC to 2 of LCD?

Thanks.

Regards,

Alpesh Mandani

Labels (1)
0 Kudos
Reply
2 Replies

594 Views
alpeshmandani
Contributor IV

Hi Artur,

Thanks for you support.

I will check in controller of LCD panel.

Thanks

Regards,

Alpesh

0 Kudos
Reply

594 Views
art
NXP Employee
NXP Employee

Actually, the possibility to communicate that way (using only 2 lanes of the i.MX6 MIPI DSI host and leaving other 2 lanes of the LCD floating) depends on the LCD itself. So, check the LCD specs first. Also, please note that the maximum display resolution, supported by the i.MX6 MIPI DSI Host module, is limited to 1280x720 pixels.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply