imx93_ota "This wic have NOT terminate tag after"

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

imx93_ota "This wic have NOT terminate tag after"

跳至解决方案
408 次查看
tgt007
Contributor II

 

I used the"./assemble_base_image.sh -e  -b imx93 "command to create the "swu_singlecopy_rescue_imx93_emmc_20240605.sdcard" file.Upgrade the "swu_singlecopy_rescue_imx93_emmc_20240605.sdcard" file using uuu.An error has occurred.

"This wic have NOT terminate tag after"

D:\share\imx-matter_2023-q4_imx8mmevk-matter>uuu.exe -b emmc_all swu_singlecopy_rescue_imx93_emmc_20240605.sdcard
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.165-0-g7347a80

Success 0 Failure 1


2:33 1/ 1 [This wic have NOT terminate tag after ] SDPS: boot -scanterm -f swu_singlecopy_rescue_imx93_emmc_20240605


D:\share\imx-matter_2023-q4_imx8mmevk-matter>pause
请按任意键继续. . .

0 项奖励
1 解答
226 次查看
hustdage
Contributor II

@tgt007  I have sent you the answer and listed all the souce code for this root cause by private message.

You can decide to public it now.

I will pubilc it later to give NXP engineer chance to really read their own code, which is existing for years.

 

 

 

在原帖中查看解决方案

0 项奖励
11 回复数
211 次查看
pengyong_zhang
NXP Employee
NXP Employee

Hi. @tgt007 

For .sdcard you need to use dd command flash it to your SD card.

 

0 项奖励
200 次查看
hustdage
Contributor II

This reply shows you  have no idea about the NXP BSP source code as a NXP engineer.

Further, the root cause is not the extension .sdcard.

In your opnion, if rename .wic to .sdcard, the image can be changed. It needs dd command.

In your mind, like a .txt file, when you rename to .mp4, it could become a movie.

 

0 项奖励
231 次查看
pengyong_zhang
NXP Employee
NXP Employee

Hi @tgt007 

Please use the "uuu -b emmc <bootloader> <rootfs.wic.bz2>" and see the result, emmc_all is for whole image.

0 项奖励
238 次查看
hustdage
Contributor II

If NXP engineers do not know their own code, then I can provide you with training and provide the answer to this question.

0 项奖励
227 次查看
hustdage
Contributor II

@tgt007  I have sent you the answer and listed all the souce code for this root cause by private message.

You can decide to public it now.

I will pubilc it later to give NXP engineer chance to really read their own code, which is existing for years.

 

 

 

0 项奖励
212 次查看
tgt007
Contributor II

thinks!

0 项奖励
275 次查看
pengyong_zhang
NXP Employee
NXP Employee
0 项奖励
368 次查看
pengyong_zhang
NXP Employee
NXP Employee

HI, @tgt007 

Where did you get this command and the shell file?

B.R

0 项奖励
343 次查看
tgt007
Contributor II
AN13872
0 项奖励
382 次查看
pengyong_zhang
NXP Employee
NXP Employee

Hi, @tgt007 

You should use emmc_all with .wic file. you can ru the uuu see more help about uuu.

B.R

0 项奖励
378 次查看
tgt007
Contributor II
How to generate WIC files.This command "./assemble_base_image.sh -e -b imx93 " automatically generates the SDCARD file.
0 项奖励