I used the"./assemble_base_image.sh -e -b imx93 "command to create the "swu_singlecopy_rescue_imx93_emmc_20240605.sdcard" file.Upgrade the "swu_singlecopy_rescue_imx93_emmc_20240605.sdcard" file using uuu.An error has occurred.
"This wic have NOT terminate tag after"
D:\share\imx-matter_2023-q4_imx8mmevk-matter>uuu.exe -b emmc_all swu_singlecopy_rescue_imx93_emmc_20240605.sdcard
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.165-0-g7347a80
Success 0 Failure 1
2:33 1/ 1 [This wic have NOT terminate tag after ] SDPS: boot -scanterm -f swu_singlecopy_rescue_imx93_emmc_20240605
D:\share\imx-matter_2023-q4_imx8mmevk-matter>pause
请按任意键继续. . .
已解决! 转到解答。
@tgt007 I have sent you the answer and listed all the souce code for this root cause by private message.
You can decide to public it now.
I will pubilc it later to give NXP engineer chance to really read their own code, which is existing for years.
This reply shows you has no idea about the NXP BSP source code as a NXP engineer.
Further, the root cause is not the extension is .sdcard.
In your opnion, if rename .wic to .sdcard, the image can be changed. It needs dd command.
Like a .txt file, when we rename to .mp4, it could become a movie.
@tgt007 I have sent you the answer and listed all the souce code for this root cause by private message.
You can decide to public it now.
I will pubilc it later to give NXP engineer chance to really read their own code, which is existing for years.