SDK:Q10.0.0_2.0.0_ANDROID_SOURCE
CPU:IMX8QX6
Use these pins of QSPI0A as ordinary IO ports in the hardware circuit. But an error was reported.
Other places that use these pins have been disabled in the device tree
fsl,pins = <
IMX8QXP_QSPI0A_DQS_LSIO_GPIO3_IO13 0x00000020
IMX8QXP_QSPI0A_DATA0_LSIO_GPIO3_IO09 0x00000020
IMX8QXP_QSPI0A_DATA1_LSIO_GPIO3_IO10 0x00000020
IMX8QXP_QSPI0A_DATA2_LSIO_GPIO3_IO11 0x00000020
>;
error log:
[ 5.599057] imx8qxp-pinctrl scu:pinctrl: pin_config_set op failed for pin 156
[ 5.606244] nvp6324_mipi 16-0030: Error applying setting, reverse things back
已解决! 转到解答。
Hi relax-wu
reason may be that these pads are used by M4 :
SDK_MEK-MIMX8QX https://mcuxpresso.nxp.com/en/welcome
(folder ../driver_examples/flexspi)
One can refer to below linik how to move some resources/pads from the M4 partition
to the A cores partition
Best regards
igor
Hi relax-wu
reason may be that these pads are used by M4 :
SDK_MEK-MIMX8QX https://mcuxpresso.nxp.com/en/welcome
(folder ../driver_examples/flexspi)
One can refer to below linik how to move some resources/pads from the M4 partition
to the A cores partition
Best regards
igor
per Android documentation (Release Notes) : Android Q10.0.0_2.0.0 (Linux 5.4 kernel)
(L5.4.3_1.0.0)
per Linux L5.4.3_1.0.0 documentation from :
Best regards
igor