Dear NXP,
I have questions for supporting rtsp streaming of camera.
I am using imx-yocto-L5.4.70_2.3.0 and image build is imx-image-full.
And I have checked libgstrtspserver-1.0.so.0 and libgstrtspserver-1.0.so.0.1602.0 in rootfs and sdk.
My question is "Should I still add "gst-variable-rtsp-server" package for rtsp streaming in imx8qxp in yocto build?"
Please help me if you have an idea.
current bsp should support gst-variable-rtsp-server already, could you use it directly?
Hi, Joanxie
That's what I am asking. When I have use "gst-rtsp-server" directly, I couldn't have succeded rtsp streaming in client side, So, I am asking another way to use "gst-rtsp-server.
Sorry, mistypo.
So, I am asking another way to use "gst-variable-rtsp-server.
the message shows that couldn't find this? try the command like this:
server:
gst-variable-rtsp-server -p 9001 -u "filesrc location=<filename.mp4> ! qtdemux ! queue ! rtph264pay name=pay0 pt=96"
client:
gst-launch-1.0 rtspsrc location=rtsp://$SERVERIP:9001/stream ! queue ! rtph264depay ! v4l2h264dec ! autovideosink