Hi
我想请教一个问题,目前处于初板开发阶段,之前都是以模块形式做的开发,初次碰到这种纯接口的通信适配
fpga获得ov2740相机的码流,并以bt1120的格式输出1080p 60fps的码流;通过转化模块 LIF‐MD6000
(由bt1120格式变成RGB888格式)变成RGB888mipi码流格式输出到 imx8qm的mipi csi接口 ,不需要spi通信提供控制,只需要识别到码流然后提供接口给应用即可
请问我需要在驱动和设备树中做哪些修改和配置来进行适配,实现imx8qm的mipi csi接口识别读取到RGB888的1080p 60fps的码流
硬件框架图如下,CL1_SPI画错了,没有这个线
内核版本为Linux version 4.14.98-imx_4.14.98_2.0.0_ga (gcc version 7.3.0 (GCC))
Any ideas for debugging or suggestions appreciated.
Thanks
zhou
you can refer to the Table 15-2. Rx Controller Core Configuration Port Descriptions, choose the correct format you need, imx8qm mipi csi supports rgb888 directly, I don't think you need to change this in the dts file
the reference manual for imx8qm hasn't been released yet, I couldn't share with you here, if you need it, pls submit a case in the nxp official website