Hi all,
I'm confused about how the interrupt sources are mapped to the IRQSTEER. Here is a use case to illustrate:
I want the M4_0 to use LSIO GPT_4. The interrupt ID of GPT_4 is 167. I could experimentally figure out that this interrupt source #167 is routed to IRQSTEER_1 and becomes vector 33 to the M4 core. But how I derive 33 from 167?
I'd appreciate it if someone could elaborate on the process or point me to relevant documentation.
Thanking you in advance,
--
TD
Hi Thierry
M4 has it's own NVIC, table below (it is from i.MX8QXP Reference Manual,
but for i.MX8QM it is the same) shows "external interrupt" vectors -
"external" interrupts are mapped to IRQSTEER module, so
IRQSTEER_1 becomes vector 33 to the M4 core.
i.MX 8DualXPlus/8QuadXPlus Applications Processor Reference Manual
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
That's interesting, thank you, Igor.
So the interrupt triggered by GPT_4 is routed to IRQSTEER_1, which then triggers interrupt 33 of the M4, as described in the table you mentioned. Do I get it correctly?
Now the question is: how comes GPT_4 is associated to IRQSTEER_1?
Thank you for your patience.
--
TD
I sent additional details via mail.
Best regards
igor
can you provide this information to me as well? I am having an issue figuring out which IRQ_STEER the Flexcan interrupts are routed too.
1. as these description,
LSIO_GPIO_INT7_IRQn is 168.
LSIO_MU5_INT_B_IRQn is 183.
these two interrupt source are corresponding to IRQSTEER_2_IRQn = 34, /**< External interrupt 2 */.
but now 168 is IRQSTEER_1, 183 is IRQSTEER_2. could you help figure out the relationship?
2. the NVIC only support 0-255 number interrupt, except for 16 core interrupt, there have 240 number interrupt, which is corresponding the code description.
__IOM uint8_t IP[240U]; /*!< Offset: 0x300 (R/W) Interrupt Priority Register (8Bit wide) */
but the external interrupt source is 384, is there have the description for the relationship fir the NVIC and external interrupt source ? now i am confused with the relationship among Shared Int Source, NVIC, and IRQ_STEER, could you have a instance for this?
thank you
Could you please elaborate ?
i working on iMX8DXL-M4, Recently encountered the same problem。
Please consider the following source code:
GPIO_PortEnableInterrupts(LSIO__GPIO7, 1 << bPinNum);
NVIC_EnableIRQ(IRQSTEER_1_IRQn);
NVIC_SetPriority(IRQSTEER_1_IRQn, 6);
IRQSTEER_EnableInterrupt(IRQSTEER, LSIO_GPIO_INT7_IRQn);
i have experiment this code is ok. I found out that M4 receives IRQSTEER_1 (which is 33) whereas LSIO_GPIO_INT7_IRQn is 168.
NVIC_SetPriority(IRQSTEER_2_IRQn, 3);
IRQSTEER_EnableInterrupt(IRQSTEER, LSIO_MU5_INT_B_IRQn);
M4 receives IRQSTEER_2 (which is 34) whereas LSIO_MU5_INT_B_IRQn is 183.
Is there a way to figure out the relation between the IRQ fired by the peripheral and the IRQSTEER_n_IRQn (n ranging from 0 to 5) ? i can't find these description in specific document.
thanks a lot for helping,
Hi Igor,
Could you please elaborate ?
Please consider the following source code:
Hi Bruno
>Is there a way to figure out the relation between the IRQ fired by the peripheral
>and the IRQSTEER_n_IRQn (n ranging from 0 to 7) ?
IRQSTEER_0 External Interrupt 0 IRQ=32 (Ints 0-63 from Table 3-4. Shared Peripheral Interrupts)
IRQSTEER_1 External Interrupt 1 IRQ=33 (Ints 64-127 from Table 3-4. Shared Peripheral Interrupts)
...
e.t.c.
Best regards
igor
Hi Igor,
Thanks for this usefull reply.
As I struggle to get the full picture on how IRQSTEER works, I have 2 others questions.
Your help is greatly appreciated,
Regards,
Bruno.
Hi Bruno
additional details were sent to your support case 00283135.
Best regards
igor
Could you make this response public?
I have the same question.
There are 594 IRQn in MIMX8QX6_cm4.h, while only IRQ_Steer manages 512.
For example I can't see how is related IRQSTEER_2_IRQn with LSIO_GPIO_INT1_IRQn