imx8mqevk svga compatible

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8mqevk svga compatible

2,663 Views
Endo1
Contributor I

I'm currently trying to connect to the display with SVGA using the imx8mqevk board, but it says "out of range" and I can't see it on the display.

What do I need to do to get it to display in SVGA?
The contents I have carried out are as follows.
Thanking you in advance.

Implementation content:

# Your i.MX Yocto Project Community BSP

Branch: imx-linux-gatesgarth
Manifest: imx-5.10.9-1.0.0.xml


# Your Linux kernel

Repository: https://source.codeaurora.org/external/imx/linux-imx.git
Tag: lf-5.10.y-1.0.0
Commit: 32513c25d8c7867f07b44900368346795357b48e


----
# Patch reference source

* Since it is for the Tradex version kernel, it could not be applied to the Community BSP version kernel as it is.

https://community.nxp.com/t5/i-MX-Processors/imx8mq-hdmi-custom-resolution-800x600-output-no-signal/...


----
#Implementation by us

* The second line of cdns-mhdp-hdmi-phy.c is https://community.nxp.com/t5/i-MX-Processors/HDMI-DRM-custom-resolution-and-clock-frequency/mp/ Calculated using the Excel file mentioned in 1029697 / highlight / true # M152124.

`` ```
diff --git a / drivers / gpu / drm / bridge / cadence / cdns-hdmi-core.c b / drivers / gpu / drm / bridge / cadence / cdns-hdmi-core.c
index 28193178140f..15c1522025c7 100644
--- a / drivers / gpu / drm / bridge / cadence / cdns-hdmi-core.c
+++ b / drivers / gpu / drm / bridge / cadence / cdns-hdmi-core.c
@@ -574,13 +574,6 @@ cdns_hdmi_bridge_mode_valid (struct drm_bridge * bridge,
if (mode-> hdisplay> 5120 || mode-> vdisplay> 2160)
return MODE_BAD_HVALUE;

-/ * imx8mq-hdmi does not support non CEA modes * /
--if (! strncmp ("imx8mq-hdmi", mhdp-> plat_data-> plat_name, 11)) {
--vic = drm_match_cea_mode (mode);
--if (vic == 0)
--return MODE_BAD;
-}
――――
mhdp-> valid_mode = mode;
ret = cdns_mhdp_plat_call (mhdp, phy_video_valid);
if (ret == false)


diff --git a / drivers / gpu / drm / drm_edid.c b / drivers / gpu / drm / drm_edid.c
index b7ddf504e024..21795f8b4d7b 100644
--- a / drivers / gpu / drm / drm_edid.c
+++ b / drivers / gpu / drm / drm_edid.c
@@ -1519,6 +1519,11 @@ static const struct drm_display_mode edid_cea_modes_193 [] = {
4272, 4400, 0, 2160, 2168, 2178, 2250, 0,
DRM_MODE_FLAG_PHSYNC | DRM_MODE_FLAG_PVSYNC),
.picture_aspect_ratio = HDMI_PICTURE_ASPECT_256_135,},
+ / * 220 --800x600 @ 60Hz * /
+ {DRM_MODE ("800x600", DRM_MODE_TYPE_DRIVER, 40000, 800, 840,
+ 850, 950, 0, 600, 603, 605, 635, 0,
+ DRM_MODE_FLAG_PHSYNC | DRM_MODE_FLAG_PVSYNC),
+ .picture_aspect_ratio = HDMI_PICTURE_ASPECT_16_9,},
};;

/ *
@@ -3323,7 +3328,7 @@ static u8 * drm_find_cea_extension (const struct edid * edid)
static __always_inline const struct drm_display_mode * cea_mode_for_vic (u8 vic)
{
BUILD_BUG_ON (1 + ARRAY_SIZE (edid_cea_modes_1) --1! = 127);
--BUILD_BUG_ON (193 + ARRAY_SIZE (edid_cea_modes_193) --1! = 219);
+ BUILD_BUG_ON (193 + ARRAY_SIZE (edid_cea_modes_193) --1! = 220);

if (vic> = 1 && vic <1 + ARRAY_SIZE (edid_cea_modes_1))
return & edid_cea_modes_1 [vic -1];


diff --git a / drivers / gpu / drm / imx / mhdp / cdns-mhdp-hdmi-phy.c b / drivers / gpu / drm / imx / mhdp / cdns-mhdp-hdmi-phy.c
index f96b200885df..6936a8419afa 100644
--- a / drivers / gpu / drm / imx / mhdp / cdns-mhdp-hdmi-phy.c
+++ b / drivers / gpu / drm / imx / mhdp / cdns-mhdp-hdmi-phy.c
@@ -58,6 +58,8 @@ static const struct hdmi_ctrl imx8mq_ctrl_table [] = {
{27000, 27000, 1250, 337500, 337500, 0x03, 0x1, 0x1, 300, 0x0EC, 0x03C, 100, 0x030, 0x030, 2700000, 2700000, 0, 2, 2, 2, 4, 0x3, 33750, 33750},
{27000, 27000, 1500, 405000, 405000, 0x03, 0x1, 0x1, 360, 0x11C, 0x048, 120, 0x03A, 0x03A, 3240000, 3240000, 0, 2, 2, 2, 4, 0x3, 40500, 40500},
{27000, 27000, 2000, 540000, 540000, 0x03, 0x1, 0x1, 240, 0x0BC, 0x030, 80, 0x026, 0x026, 2160000, 2160000, 0, 2, 2, 2, 4, 0x2, 54000, 54000},
+ {40000, 40000, 1000, 400275, 400275, 0x05, 0x1, 0x1, 593, 0x126, 0x127, 80, 0x026, 0x026, 3202200, 3202200, 1, 1, 1, 1, 1, 0x3, 40027, 40027} ,,
+ {40000, 40000, 1000, 400275, 400275, 0x05, 0x1, 0x1, 593, 0x1D7, 0x076, 80, 0x026, 0x026, 3202200, 3202200, 1, 2, 2, 2, 4, 0x3, 40027, 40027} ,,
{54000, 54000, 1000, 540000, 540000, 0x03, 0x1, 0x1, 480, 0x17C, 0x060, 80, 0x026, 0x026, 4320000, 4320000, 1, 2, 2, 2, 4, 0x3, 54000, 54000},
{54000, 54000, 1250, 675000, 675000, 0x04, 0x1, 0x1, 400, 0x13C, 0x050, 50, 0x017, 0x017, 2700000, 2700000, 0, 1, 1, 2, 4, 0x2, 67500, 67500},
{54000, 54000, 1500, 810000, 810000, 0x04, 0x1, 0x1, 480, 0x17C, 0x060, 60, 0x01C, 0x01C, 3240000, 3240000, 0, 2, 2, 2, 2, 0x2, 81000, 81000},
@@ -149,6 +151,7 @@ static const struct hdmi_pll_tuning imx8mq_pll_table [] = {
{10, 4455000, 4455000, 0x5, 0x3, 0x0, 0x07, 0x0F, 660, 0x4C, 219, 7, 272},
{11, 4950000, 4950000, 0x6, 0x3, 0x1, 0x00, 0x07, 550, 0x42, 213, 7, 258},
{12, 5940000, 5940000, 0x7, 0x3, 0x1, 0x00, 0x07, 660, 0x42, 244, 8, 292},
+ {13, 3202200, 3202200, 0x6, 0x3, 0x1, 0x00, 0x07, 593, 0x4C, 203, 7, 256}, / * nominal VCO freq: 3202200 * /
};;

/ * HDMI TX PLL tuning settings, pixel clock is input * /
`` ```

0 Kudos
Reply
11 Replies

2,651 Views
joanxie
NXP TechSupport
NXP TechSupport

do you mind sharing the logfile and your xls file with pixel clock calculation with me? let me check if your pixel clock setting is correct or not

 

0 Kudos
Reply

2,642 Views
Endo1
Contributor I

Share log and xls files.

0 Kudos
Reply

2,631 Views
joanxie
NXP TechSupport
NXP TechSupport

refer to your VOC, try to use this:

{ 14, 3202.1, 3202.3, 0x6, 0x3, 0x1, 0x00, 0x07, 593, 0x4C, 203, 7, 256 }, // nominal VCO freq: 3202.2

0 Kudos
Reply

2,614 Views
Endo1
Contributor I

I tried it but the problem didn't go away.

I also tried fixing vco_freq_min / vco_freq_max in imx8mq_ctrl_table, but that didn't fix the problem either.

Is there anything else I can try?

 

0 Kudos
Reply

2,600 Views
joanxie
NXP TechSupport
NXP TechSupport

refer to your calculate xls file, the pixel clock is 40028, how about change the 40000 to 40028? and try another 40014 and voc as below
165     { 19, 4001.3, 4001.5, 0x5, 0x3, 0x0, 0x07, 0x0F,  741, 0x42, 184, 6, 226 }, // nominal VCO freq: 4001.4

 

0 Kudos
Reply

2,585 Views
Endo1
Contributor I

I did what I was told, but the SVGA mode became unavailable and the problem was not resolved.
Maybe my implementation is bad.
I will attach a log, so please let me know if you notice anything.
Best Regards

0 Kudos
Reply

2,580 Views
joanxie
NXP TechSupport
NXP TechSupport

did you check pixel clk,phy clk from clk_summary? if no, pls dump them and check it

 

0 Kudos
Reply

2,555 Views
Endo1
Contributor I

Dumped clk_summary. The Reference Clock is 27MHz and the Pixel Clock is 40.00MHz, which looks fine.

> phy_27m 2 2 0 27000000 0 0 50000
> video2_pll1_ref_sel 2 2 0 27000000 0 0 50000
> video2_pll_out 1 1 0 40000000 0 0 50000

0 Kudos
Reply

2,550 Views
joanxie
NXP TechSupport
NXP TechSupport

could you confirm that your display can boot up successfully from other platform? I confirmed from vendor that they couldn't guarantee the display which isn't in the table can be boot up successfully , they only support the display can be found in the clock table

 

0 Kudos
Reply

2,525 Views
Endo1
Contributor I

If another platform is connected to the display, it will be displayed.
I understand that we do not guarantee displays that are not on the table.
thank you.

0 Kudos
Reply

2,628 Views
Endo1
Contributor I

thank you.
I will try.

0 Kudos
Reply