Hi,
according to the TRM 14.1.2.1 Decoder Features Hatro G1 in i.MX8MQ supports scaling:
• Video post-processing features
• Frame scaling with maximum up-scaling factor of 3
But in the Synthesis configuration register post-processor (SWREG100)
38300190: e0c75000
the SW_PPD_SCALE_LEVEL is 0 - meaning PP did not have scaling support? This is read by the imx-vpu-hantro software and my PP config is rejected.
Am I overlooking something? (No, I can't use GPU!)
已解决! 转到解答。
Questions was if this is enabled in i.MX8MQ? Do you have any information about how to enable scaling with the PP?
If I disable the scaling enabled check in imx-vpu-hantro software I get a decoder error...