imx8m mini with FLEXSPI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8m mini with FLEXSPI

Jump to solution
2,813 Views
Abdellahkafi
Contributor I

Hi,

I want to use FlexSPI on the imx8m mini. It seems working but when i write bock of data ,i have noticed that writing data to FlexSPI  TX IP FIFO is really slow, in my case writing 32 bytes needs around 4 us, also when i try to toggle GPIO by directly writing to the dedicated register takes long time (150 ns , the assembly code looks fine with only 3 instructions) which seems too slow, i tried also to fire a timer interrupt to be sure that clock/pll configurations are fine. 

All the tests are made on the M4 core and the code is based on the SDK_2.8.2_EVKB-IMXRT1050; so i am wondering what is the time needed  to access peripherals registers.

 

 

Labels (1)
0 Kudos
Reply
1 Solution
2,799 Views
igorpadykov
NXP Employee
NXP Employee

Hi Abdellahkafi

 

regarding "time needed  to access peripherals registers" - general answer

this is caused by bus arbiters, like NIC301 in i.MX6 processors, similar modules

are used in i.MX8 processors. Good latency description can be found in 

sect.3.4 NIC transfer latency AN4947 "Understanding Vybrid Architecture"

https://www.nxp.com/docs/en/application-note/AN4947.pdf

So 150 ns for toggling GPIO by directly writing to the dedicated register may be

considered as normal.

 

Best regards
igor

View solution in original post

0 Kudos
Reply
2 Replies
2,800 Views
igorpadykov
NXP Employee
NXP Employee

Hi Abdellahkafi

 

regarding "time needed  to access peripherals registers" - general answer

this is caused by bus arbiters, like NIC301 in i.MX6 processors, similar modules

are used in i.MX8 processors. Good latency description can be found in 

sect.3.4 NIC transfer latency AN4947 "Understanding Vybrid Architecture"

https://www.nxp.com/docs/en/application-note/AN4947.pdf

So 150 ns for toggling GPIO by directly writing to the dedicated register may be

considered as normal.

 

Best regards
igor

0 Kudos
Reply
2,793 Views
Abdellahkafi
Contributor I

Thanks for your fast answer

Concerning FlexSPI, writing 32 bytes (eight 32-bits words ) to IP TX-FIFO, I changed the watermark level to 3 in my case and the filling time is around 2.5 us, is it expected and is there any way to make it faster without using DMA?

Best regards 

0 Kudos
Reply