imx8 m plus - XDP support on ENET

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8 m plus - XDP support on ENET

1,171 Views
NG_R3
Contributor I

Hi there,

 

I'm working on a iMX8M plus based board on which I'm running Linux. The ENET is driven by the FEC Linux driver which doesn't support XDP. I see that dpaa2 has integrated XDP support. Is it possible to somehow get an XDP program running on this driver and filter packets arriving on the ENET?

Thanks,

 

Nir 

Labels (1)
0 Kudos
Reply
5 Replies

987 Views
NG_R3
Contributor I

Hi,

Can you please relate to the following link?

[PATCH v5 0/3] net: fec: add xdp and page pool statistics (kernel.org)

When will XDP support for fec driver be integrated into the mainline or imx kernel?

Thanks,

Nir.

0 Kudos
Reply

1,148 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Are you using the NXP reference board? Which version BSP are you using?

0 Kudos
Reply

1,143 Views
NG_R3
Contributor I

Hi,

I'm not using the iMX8M plus evaluation board.

The Linux OS is built by a Yocto project based on NXP provided meta-layers, Yocto version is hardknott.

The Linux kernel version is 5.10.109, PREEMPT_RT patched.
The board is fully functional. I need to run XDP filtering capabilities on the ENET driver.

Thanks,

Nir.

0 Kudos
Reply

1,130 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

I think it is the question about the linux, you can google it to see more method and advice. Sorry about it.

0 Kudos
Reply

1,116 Views
NG_R3
Contributor I

I understand.

Can you check if there is any plan or timeline to add XDP support to the FEC Linux driver?

If not, can you give a contact to someone that can assist with this task?

Thanks.

0 Kudos
Reply